Toshiba Satellite C875D-S7105 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop for the Price

POSTED BY: B-Lady , Burlington NC
Overall rating: 5 out of 5 5 out of 5

This is only the second laptop I have owned. I have a Toshiba laptop at work and I love it. The one I just purchased for personal use is very close to the same model and I love the features, especially the numeric keypad. I was not prepared to dive into Windows 8 which came pre-loaded, but I am getting used to it.

nice laptop

POSTED BY: dotso10 , Maynard, Mass
Overall rating: 5 out of 5 5 out of 5

its a nice laptop. light wieght. easy to handle . the price was great.

Very easy to use, once I got use to windows 8.

POSTED BY: Texas Angel
Overall rating: 5 out of 5 5 out of 5

I really enjoy using a laptop. I can take it with me where ever I go.

Toshiba Laptop

POSTED BY: Elsa , Brownsville, Texas
Overall rating: 5 out of 5 5 out of 5

I never had a hard time with it.

Great Laptop, I bought two!

POSTED BY: db , louisa, va
Overall rating: 5 out of 5 5 out of 5

The price was wonderful. Bought one for my husband too. Love my big beautiful screen, keyboard is calibrated for easy, smooth use, all updated technology. My one complaint: When setting it up for myself, it downloaded LOTS of unwanted programs including something called otshot that even my computer tech can not uninstall. Booooo!

Excellent Product

POSTED BY: Voltaire , Renton
Overall rating: 5 out of 5 5 out of 5

Excellent Product that efficiently and expeditiously provides a variety of useful applications and utilities for entertainment, education, professional means and ends, and personal business,

No complaints here!

POSTED BY: Gibby , Britton, MI
Overall rating: 5 out of 5 5 out of 5

This computer gives you the most bang for your buck. Period.

New Laptop with Windows 8

POSTED BY: EarthlyTreasures , Columbus, OH
Overall rating: 4 out of 5 4 out of 5

I am very impressed with the Toshiba laptop. It was rather inexpensive, but is very comparable to a "higher-end" laptop that I use for work. I also love the new Windows 8! Graphics are also awesome.

thank you

POSTED BY: elaine , Highland, NY
Overall rating: 4 out of 5 4 out of 5

waiting for windows 8 for dummies book as promised when lap top registered

Good for sitting around and taking on trips

POSTED BY: firestorm , Tennessee
Overall rating: 4 out of 5 4 out of 5

This model is not for the gaming, business class type person. Would up grade. But, it keeps me in the same room with the family when something at work does have to be looked at quickly. PLEASE tyr TREND as the virus, I went ahead and subscribed to Norton. It is junk. I am in security in the IT field. Would not trust Norton, when the year runs out will put this on my TREND account. Thought I would give it a shot and spent money I really did not need to. Sorry I did....

Good laptop. Awful OS

POSTED BY: Ismael , Redlands, CA
Overall rating: 4 out of 5 4 out of 5

No complaints with the laptop. I like it so far. But the Windows 8 operating system is a pain. It looks like it is designed to work well with a touch-screen, but in this laptop it does not make much sense to have it. I systematically go into the old fashion Desktop-style mode but as soon as I move my mouse to the edge of the screen I get Windows 8 menus that I do not want to use. If I could change the OS I would.

Nice Laptopize

POSTED BY: dwuker , Miami, Florida
Overall rating: 4 out of 5 4 out of 5

This is my first laptop. I like the size of the screen and the price I paid for it.

Software that Was not

POSTED BY: Arlene , Los Banos, CA
Overall rating: 4 out of 5 4 out of 5

I don't like the fact that the Microsoft package was not pre-installed and that we had to download it from the website. The computer should come with everything that is needed so we can use it straight out of the box.

Econamy

POSTED BY: Ravi , Sterling,VA
Overall rating: 4 out of 5 4 out of 5

Good performance with great utility for itscomparative price.

good value laptop

POSTED BY: geeeburger , tuckerton, nj
Overall rating: 4 out of 5 4 out of 5

use the computer for internet mostly- and the laptop is sufficient- added 4gb more memory to bump up performance. love the 17" screen- bigger is better....if your looking to use for business- might want to upgrade, but for basic, everyday use, could not beat for the price

a real good computer

POSTED BY: joe , chihuahua, mexico
Overall rating: 4 out of 5 4 out of 5

i think this is my best computer option for a cheap price, agood deal!!!!!!!!

TRY AGAIN WITH WINDOWS

POSTED BY: CHARLY , PHOENIX
Overall rating: 4 out of 5 4 out of 5

what I DONT LIKE IS WINDOW 8, I NEED A START BUTTON.THE OLD SYSTEM WORKED WELL ,THE CHARM ,CONNEDED TO THE TOUCH PAD IS A BIG THUMBS DOWN.I HAD TO BUY A MOUSE TO HELP THE PROBLEM.I HEARED THAT YOU HAVE TO GIVE IT TIME,BUT HAS THE TIME. SO WHAT I AM SAYING IS MAKE WINDOW EASYER TO USE NOT HARDER. BUT ALL EN ALL TOSHIBA A FINE COMPUTER.

POSTED BY: lightfoot , illinois
Overall rating: 4 out of 5 4 out of 5

Good price for a good computer. Mouse is not that good

unsure

POSTED BY: KimberlyD , Summerdale al
Overall rating: 4 out of 5 4 out of 5

I would like to say that I completely love my laptop. The problem is I have had it for a month and my hardrive has crashed. Other than that I am inlove with it. I've only ever owned toshibas and would love to stick with them and probably will even after this slight inconvenience.

Good laptop

POSTED BY: ising , OH
Overall rating: 4 out of 5 4 out of 5

Windows 8 has been a challenge, but I am happy with Toshiba Satellite.

great laptop value

POSTED BY: jm , new Hampshire
Overall rating: 4 out of 5 4 out of 5

Laptop is a very good value - does everything the average user needs and is plenty fast. Only downside is windows 8 - I hate it (not the fault of the laptop). If I had wanted a laptop that works like a mac I would have bought a mac.

Great laptop

POSTED BY: Suji , Cathedral City, CA
Overall rating: 4 out of 5 4 out of 5

Beautiful large screen with excellent resolution. Good value for the money. My only issue is with the Windows 8 program that came with the laptop. Windows 8 was a program purposed for touch computers. Because my new laptop was not a touch computer there were some complications and changes that needed to be made, extra steps taken, delays in loading, and just extra trouble that I didn't need. Once I made all adjustments, it worked well for me and I enjoy it very much.

Good laptop, but keyboard.needs some help

POSTED BY: Bridge , Miami, FL
Overall rating: 4 out of 5 4 out of 5

Good computer, but the keyboard and mouse right and left click buttons are too hard to push down when typing and there is not obvious way to adjust the keyboard touch like there was in other computers (control area). This is a SERIOUS issue that needs addressing.

Disappointing

POSTED BY: Maddy , San Francisco, CA
Overall rating: 3 out of 5 3 out of 5

The mouse pad is not very sensitive, tends to get "stuck," and the keyboard "bounces" as I type. Both are bad enough that I'm considering getting a wireless keyboard and mouse to use with my laptop when I'm at home.

OK laptop

POSTED BY: doright , anywhere florida
Overall rating: 3 out of 5 3 out of 5

Although I am happy with windows 8, the laptop itself seems to be cheaply made. My last laptop was sturdy, but this is plastic and sometimes the keys stick, especially the space bar. If I were to purchase another laptop I would look for one that was stronger and not a cheap plastic.

OK starter laptop

POSTED BY: Con man
Overall rating: 3 out of 5 3 out of 5

This is just a starter laptop, nothing special at all.

Toshiba

POSTED BY: SaintJohn159 , Girard, OH
Overall rating: 3 out of 5 3 out of 5

The computer is fine. Windows 8 is absolutely terrible! Not at all user friendly.

good so far

POSTED BY: Hillbilly , South Carolina
Overall rating: 3 out of 5 3 out of 5

So far no problems with the lap top. A Lack of some base office / word programs that were included on previous laptops is about the only downside I have found so far. Purchased laptop for my 7th grade daughter as a quick replacement for her old one that bit the dust.

POSTED BY: nazer
Overall rating: 2 out of 5 2 out of 5

No instructions are learning diagrams.. not happy about windows 8 and my employer program is not up to date with new system, therefore I can not use this computer for my work base training

Where Is the scroll on touchpad?

POSTED BY: Tulips2u , Fremont, CA.
Overall rating: 2 out of 5 2 out of 5

Have been using this for 2 weeks now. I had to plug in a mouse because I can't scroll with my finger. I don't like the screen going light/dark while charging it. I find this hard on my eyes. As for the Win 8, I enjoy the challenge of a new OS, but I think Win 8 is better suited for a touch screen. Love the big screen. Thinking about adding more memory. Hope it will speed things up....

Dead Battery

POSTED BY: v
Overall rating: 2 out of 5 2 out of 5

Laptop stopped working within 2 h of getting it. Took it back to BB and they said battety was not installed properly....took it back and it failed agin in 2 h. Bought a Dell!

SoSo

POSTED BY: Lola , Thornton, CO
Overall rating: 2 out of 5 2 out of 5

The computer is slow, the key board is bad and to top it all off Windows 8 is the worst thing Microsoft has ever done.

MSRP: $467.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core A6-4400M Accelerated Processor
  • Windows 8
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Wi-Fi® Wireless networking (802.11b/g/n)

shop for accessories