Toshiba Satellite C875D-S7330 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

my review

POSTED BY: willie , columbus ohio
Overall rating: 5 out of 5 5 out of 5

2nd Toshiba laptop I've owned and it's great

Toshiba Satellite

POSTED BY: ablebody , Beattyville KY
Overall rating: 5 out of 5 5 out of 5

easy to use , bright screen, great service

cant beat it

POSTED BY: buckysrun , chesterfield,va
Overall rating: 5 out of 5 5 out of 5

I've tried others but nothing compares to a Toshiba

Excellent product for what i needed it for.

POSTED BY: lonewolf45
Overall rating: 5 out of 5 5 out of 5

it is an excellent laptop although I found it hard to navigate at first because it was my first time using windows 8. I would still rather have window 7

Laptop

POSTED BY: Tankmgr , Lutz, FL
Overall rating: 5 out of 5 5 out of 5

Still learning but so far I've been very satisfied with the performance and options offered.

spectacular

POSTED BY: Lor , Wilkes-Barre, PA
Overall rating: 5 out of 5 5 out of 5

this is my first laptop ever, couldn't have chosen one better.

Great Product

POSTED BY: acohorn , West Alexandria, OH
Overall rating: 5 out of 5 5 out of 5

My children and I all use this laptop, we all love it. It works great for school work and takes up very little space. I can run the battery to 7% and it takes about 30 minutes to get back to a full charge!!! Great Product!!

Good laptop for the money

POSTED BY: Newbie Laptop Guy , VT
Overall rating: 5 out of 5 5 out of 5

This is the first laptop I've owned and it runs well so far. I'm not a whiz on computers who does all kinds of complicated stuff with a laptop, but for my uses--word processing and surfing the internet, it works fine and runs much quicker than my old computer. The large screen size is nice--I use the laptop as a desktop plugged into a keyboard, but have the flexibility to take it with me if I go somewhere.

nice laptop

POSTED BY: me , michigan
Overall rating: 5 out of 5 5 out of 5

nice

good laptop for money

POSTED BY: jimbo , albin wyo.
Overall rating: 5 out of 5 5 out of 5

good laptop, should consider providing win. 7disc to replace win 8, its a joke......provides ample keys in addition to every day usage.

Great Laptop and Windows 8 Is Simple

POSTED BY: Boss
Overall rating: 5 out of 5 5 out of 5

Am going to be short and direct, i got this laptop recently and it looks really Good, the features are very Good and very fast. Windows 8 is great and the same with windows 7 except for the difference in the start menu but i like the start menu of windows 8 better, anyone that has used windows 7 shouldn't have any problem using windows 8. I didn't get to read any book before i figured out how to use it although is my first time of using windows 8 but am in love with it as i maneuver like a pro. I was a bit skeptical from reviews i have read about windows 8 but i now know they are wrong or they are not windows conversant.

Great Laptop

POSTED BY: Lleadft , Dumfries,Va
Overall rating: 5 out of 5 5 out of 5

I bought this laptop for my daughter for Christmas and I really liked it and so when my laptop died I bought the same one for myself and I still like it.

Love it

POSTED BY: Candy , Woodbridge, VA
Overall rating: 5 out of 5 5 out of 5

Great performance, battery life and features. I'm satisfied with my laptop.

Excellent Value

POSTED BY: TJ , Cleveland, OH
Overall rating: 5 out of 5 5 out of 5

I am very satisfied with my Toshiba Laptop. It has more features for a better price than other brands I have shopped and I love the big keyboard, crystal clear screen and numeric keypad. This model's performance is more than adequate for everyday use.

Toshiba Satellite Laptop

POSTED BY: LT. , Marion, Iowa
Overall rating: 5 out of 5 5 out of 5

I personally like the larger screen and thinner dimension of the machine. Easy to read and lighter weight.

Perfect Laptop

POSTED BY: gebrown2 , San Antonio
Overall rating: 5 out of 5 5 out of 5

This laptop is perfect for my needs. It is fast and has ample storage. I can't comment on the battery life because I have never used it on battery power only.

AWESOME

POSTED BY: #1 grandma , Lucerne, CA
Overall rating: 5 out of 5 5 out of 5

I love this laptop! It's light weight, slim design makes it easy to carry along anywhere. The key pad is easy to read and type on. The brightness of the screen is a wonderful bonus!

Great laptop

POSTED BY: TLindsey , Texarkana, TX
Overall rating: 5 out of 5 5 out of 5

Great laptop for price, I use it for home stuff mainly but I also do some work on it. I love love love the 17.3 in screen!! The processor runs pretty fast also. Thanks Toshiba!!

User Friendly

POSTED BY: Solid Gold , Las Vegas, NV
Overall rating: 5 out of 5 5 out of 5

I am enjoying the benefits of Windows 8, the only problem is some of the sites I go to do not support it. They need to catch up. I love the computer. The screen is gorgeous.

my new computer

POSTED BY: justme , hondo, tx
Overall rating: 5 out of 5 5 out of 5

I love my new computer. If you get another computer, check it out.

Second time is a charm!

POSTED BY: Dr. J , Orlando, Fl
Overall rating: 5 out of 5 5 out of 5

This is my second Toshiba and I am equally satisfied. The value for dollar spent was top shelf. Screen is dynamic

Very nice Laptop

POSTED BY: Jimbo , Seguin, TX
Overall rating: 5 out of 5 5 out of 5

Very nice laptop, bright screen, long battery life, I would like it better if it had Windows 7. It has lots of memory, large harddrive, and full keyboard. So far, no problems.

top of the line in computers

POSTED BY: grannie , doniphan, mo.
Overall rating: 5 out of 5 5 out of 5

I love it, can't say more than that bu I would say this cant' be beat for the price

POSTED BY: noli , Calamba City Laguna Philippines
Overall rating: 4 out of 5 4 out of 5

contrary to other review, I like windows 8. Satellite C875 - thumbs up.

TOSHIBA C870 Series

POSTED BY: Stretch , Greensboro, NC
Overall rating: 4 out of 5 4 out of 5

My wife and I have found the Toshiba itself pretty easy to use. It does seem to be super sensitive while moving the cursor. Programs will open or icons will move from the sides of the machine when just passing over the screen. Gets quite frustrating..... The real problem for easy operation is the Windows 8 program. It is not easy to use or follow - very user unfriendly, requiring multiple steps where the prior programs only required one or two to complete a task.

Mele

POSTED BY: jjm3wife , Tucson, AZ
Overall rating: 4 out of 5 4 out of 5

I received this laptop for my birthday and used it only a few days when it wouldn''t come on

seems ok

POSTED BY: Rick , Millersview Tx
Overall rating: 4 out of 5 4 out of 5

Haven't had it long enough to give you anything detailed

Good laptop

POSTED BY: Ivy , Milwaukee, WI
Overall rating: 4 out of 5 4 out of 5

It is an excellent laptop with a small problem with the mouse. However, this laptop had a very sleek design; I would like the battery to last a little longer. Overall this a good computer for the a Toshiba laptop.

better than what I had

POSTED BY: Grandma , Richmond, Indiana
Overall rating: 4 out of 5 4 out of 5

It is like anything else new, you just have to make up your mind to get used to the changes.

Big screen laptop

POSTED BY: Razorback65 , Canton, Mississippi
Overall rating: 4 out of 5 4 out of 5

My 2nd Toshiba, other is a 15 " screen. This 17" is so much better, fast downloads, sets up easily. Only con is Windows 8, but it comes on all brands of computers.

So Far, So Good

POSTED BY: Black Pearl , Montana
Overall rating: 4 out of 5 4 out of 5

So far, so good. The on-board mouse pad was very sensitive and the cause of many mistakes. Once I got an external mouse, all went well. Saying that understand I am an old duffer and not real handy. But so far, I am pleased.

Very Good Laptop

POSTED BY: Dubhead42 , Ft. Lewis, WA
Overall rating: 4 out of 5 4 out of 5

The screen size and features of this laptop are amazing. It's battery life is a little weak, but the laptop makes up for it with it's performance. There has been minor software issues, but I believe that is simply because Windows 8 is still in it's early stage. When I tell how much I paid for this computer most people don't believe me. I highly recommend it. Yes it is not the top of the line can play any video game laptop. However for business, catching up on the news, watching streaming media, and running multiple tasks I would highly recommend this laptop.

Bangs & Bucks...

POSTED BY: mcrs , SouthCentral Ok
Overall rating: 4 out of 5 4 out of 5

I've owned a number of computers in the last 30 years, desktops and laptops both by a number of manufacturers, but so far, I am very well satisfied with this machine. It is fast, predictable, has a long battery life (when managed well), it has all the features and functionality that I require. It came with a great warranty, and thus far has performed above my expectations for a price well below what I had found comparable models for. Yes, I'm pleased and WILL recommend your machine to others.

Okay Laptop

POSTED BY: Bobbie , NorthCanton, OH
Overall rating: 3 out of 5 3 out of 5

Laptop not easy to use unless you are a computer expert. I absolutely hate Windows 8. Battery life not good. Would still have my last Toshiba but internet explorer and Java have serious issues. Makes me doubt the reliability of the computer.

Disappointed

POSTED BY: a
Overall rating: 3 out of 5 3 out of 5

This is my 2nd Toshiba Laptop because I love the product. However I am disappointed not with the Toshiba Product but the Windows 8 that came installed on it. I would like to revert to Windows 7. I cannot see basic programs that usually come with a computer. Also I would like very much to see a physical button to turn "On" & "Off" the Wireless connection. I am very uncomfortable with the fact that someone else has access to my computer at all times.

operating system

POSTED BY: butterfly , ohio
Overall rating: 3 out of 5 3 out of 5

came with windows 7 which is a bit difficult to navigate and the computer seems a bit sluggish for a new machine. Had trouble with internet explorer freezing up and rebooting so switched to firefox. The computer seems okay, just have to learn a new system

returned

POSTED BY: firefighter1402 , ocala,fl
Overall rating: 2 out of 5 2 out of 5

returned laptop because it was not compatiable with current system. did not like the windows 8 system at all would have kept it if it had had windows xp ro 7.

hate new things--I'm old

POSTED BY: cookie , Wauconda, IL
Overall rating: 2 out of 5 2 out of 5

Maybe it isn't the laptop but I HATE THE WINDOWS 8 SET-UP. GO BACK TO THE OLD START THEN PRESS WHAT YOU WANT! Laptop itself seems to be good but I installed a mousse-don't like to touch pad or the touch screen. Can you tell--I'm old!

I hate windows 8!

POSTED BY: Jeanie Baby , Roanoke, VA
Overall rating: 2 out of 5 2 out of 5

If I I had known what window 8 is, I would not have purchased this computer. It is very difficult to use and I have heard this comment from several people, even the people that sold it to me. They didn't bother to mention it until I had made the purchase and transferred my data and tried to use it. I liked Windows 7 - very user friendly.

MSRP: $499.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core A4-4300M Accelerated Processor
  • Windows 8
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Wi-Fi® Wireless networking (802.11b/g/n)

shop for accessories