Toshiba Satellite C875D-S7345 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Special offers

POSTED BY: Dallas Cowgirl , Bristow, VA
Overall rating: 4 out of 5 4 out of 5

I never could download my free copy of Windows 8 for Dummies, so went out and bought it. You don't make things easy to download!

Good - but wish it had more RAM

POSTED BY: TheElder , Maine
Overall rating: 4 out of 5 4 out of 5

works well enough, but with Win8 and only 4GB of ram it does seem a tab bit slow at times. Wish it had 6GB of ram, will probably up the ram later.

Mediocre at best

POSTED BY: MTF , VA
Overall rating: 2 out of 5 2 out of 5

If all you need to do is surf the internet and do microsoft office this confuzer should suffice. However, this machine won't even display the screen saver, not enough processing power. But it is cheap...the company spared no expense....lol

NOT TOO HAPPY

POSTED BY: willie , portland maine
Overall rating: 2 out of 5 2 out of 5

This is my 1st ever laptop but it should work a lot better than it does..I'm not too happy with it

BAD Buy

POSTED BY: Jess , South Jersey
Overall rating: 1 out of 5 1 out of 5

I originally got this computer for Christmas, opened the box, and was happy to see a nice sized screen and a good looking computer. I quickly came to realize that the disk drive was not put on correctly and was hanging out. GREAT! Time for a return. I had no problems returning the laptop and getting another one. My SECOND Toshiba laptop seemed to be working okay for about the first day, and then BAAM! I noticed the battery life was not normal at all for a Toshiba, and then it constantly kept telling me to restart the laptop and was operating very, very slow plus freezing. So just today I got a popup telling me that the battery life was poor, and the battery would need to be replaced. ARE YOU KIDDING ME? This time I will not be getting another Toshiba, I will be getting money back and going with something else.

MSRP: $459.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core E1-1200 Accelerated Processor
  • Windows 8
  • 4GB DDR3 1600MHz memory
  • AMD® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories