Toshiba Satellite Click W35Dt-AST2N01 Laptop

Average Customer Rating:
Free ground shipping on laptops $499+

Limit 1 per household

Some accessory offers are valid only at time of PC purchase

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Toshiba Click: Well worth the money!

POSTED BY: SquidInTheTub , Minnesota
Overall rating: 4 out of 5 4 out of 5

I believe that this convertible has the most potential of all the computers I have looked at so far. Truly, for the money, no one is offering the amount of computer that Toshiba is: 500 Gigabytes hard drive when all the others are offering maybe 32-64 Gigs. The screen size is also a bonus, and frankly, it is not as heavy as it may seem due to its size. It is actually lightweight. My only concern so far is the computer's battery life. Perhaps I got a bad battery but mine did not last anywhere near the time listed online. So, for the money and for anyone wanting the benefits of a convertible, this is the one I would suggest.

do not buy

POSTED BY: jesus , chantilly .VA
Overall rating: 3 out of 5 3 out of 5

I buy it because it looked better than the Microsoft Surface, but it's way too slow and only use it to watch youtube and read news, I can not put games, very slow, this is my review of this notebook, I hope not to offend anyone.

SelfDischarging and Static electricity!

POSTED BY: JGMonarcas , Valparaiso, Chile
Overall rating: 3 out of 5 3 out of 5

SelfDischarging battery. If the computer is off and disconected, the battery goes to 90% in 5-6 h. Also very noticeable static electricity on the case when connected to A/C converter. It was a matter of designing it with case connected to earth and an earth plug in the A/C converter!!

Nice but unusable device

POSTED BY: GermanCustomer , Germany
Overall rating: 2 out of 5 2 out of 5

The click has a nice design and, from an external point of view, a very interesting product. However, the rapid self-discharging battery (in switched off mode), the electric surface tension if power is plugged and the very slow processor destroys the first look advantages. Interesting for me was to hear that the battery discharging (about 30% in 1 day) and the remarkable electric surface tension is within Toshibas parameter. OK, a mobile device that consumes power for nothing – this really safes the environment.

Notebook without Battery

POSTED BY: BavarianRating , Germany
Overall rating: 1 out of 5 1 out of 5

Nice design, good form factor (13.3"), smart solution (detachable). These are the good things. However, really bad are the battery, which quickly discharge even though it is switched off (3 days and both batteries are empty). During charging the back side of the tablet is under power tension (really inconvenient). Last but not least, the processor is unworthy.

Do not buy ever

POSTED BY: scanbix , Lithuania
Overall rating: 1 out of 5 1 out of 5

I bought this for my parents as a replacement for loud, hot HP notebook. Good points regarding previous: silent-no fan, good webcam. Everything else is awful: CPU - too slow. Overall experience is just too slow. Battery life on tablet - 3 hours with such slow CPU?! Mechanical hard disk these days? I would prefer to have half of 500GB, but SSD or at least hybrid disk. Heavy!!! YOu can find ultrabooks for similar price which will be lighter, faster, and thinner. And the worst part is keyboard - it bends when you use it, keys are so unpleasant to type, very shallow keys.
  • $899.99
  • -$300.00
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • $
  • $599.99
  • »
  • Free Ground Shipping

add to cart
  • Laptop summary This product is prebuilt.
  • AMD Dual Core A4-1200 Accelerated Processor
  • Windows 8
  • 4GB DDR3L 1066MHz (Memory is not user replaceable)
  • AMD® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive
  • Wi-Fi® Wireless networking (802.11b/g/n)
  • Bluetooth® V4.0
  • Keyboard Dock: Raised Tile Keyboard, Click pad pointing device with Windows 8 gesture control, and Eject Button
  • Power Button
  • Volume Control (Up & Down)
  • Dual Lithium Ion (23.6Wh, 2-Cell)—*Not user replaceable
  • Keyboard Dock: 1 USB 3.0 port with USB Sleep and Charge, DC-in, and Docking connector
  • Tablet: Micro USB
  • Accessories Added: