Satellite E105-S1802

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Not One Complaint

POSTED BY: Cooper , Kinnelon, NJ
Overall rating: 5 out of 5 5 out of 5

I read many computer/laptop reviews before I purchased the E105...I'm glad that I did. It is the best laptop for the money, and has great features. I bought it retail, but that to me doesn't matter. Toshiba has given itself a leg above with this model. I love the backlight and long battery life.

Amazing Laptop!!!

Overall rating: 5 out of 5 5 out of 5

This Laptop is amazing, no more words... =D

Good value for money!

POSTED BY: PC Guy , Honolulu, HI
Overall rating: 4 out of 5 4 out of 5

This is my second Toshiba laptop. My first one (also with Windows Vista) is still working great; but I needed a second laptop; so I decided to buy another Toshiba. So far I am very happy with this E105; my only complain is that the speakers are of poor quality; however, when I use headphones or external speakers, the sound quality is excellent. Other than that, I love this laptop for its speed, huge hard drive, excellent memory, and great performance.


POSTED BY: Jeego , Jamaica, WI
Overall rating: 4 out of 5 4 out of 5

The Satellite E105 series, is a very thin and lightweight laptop. I would recommend this laptop to anyone that wants to not travel with a heavy load. The programs are easy to use. The only faults i find with this laptop are: the battery only lasts four hours and the speakers are way too low.

Great slim laptop

POSTED BY: JJLUZ , Wilmington, DE
Overall rating: 4 out of 5 4 out of 5

This is a very nice slim laptop that does the job. I really like the back lite keys and speed of everything. Little costly but I think it was a good buy.

Hardrive Dead in 7 months

Overall rating: 1 out of 5 1 out of 5

Bought this computer, downloaded nothing, basically just used Microsoft Word for class, and the hard drive died in seven months.

MSRP: $949.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor P7450
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 800MHz memory
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless-LAN (802.11b/g/n)

shop for accessories