Toshiba Satellite E45T-AST2N01 Ultrabook™

Average Customer Rating:
Free ground shipping on laptops $499+
up to $50 OFF Microsoft Office

Limit 5 per household

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop

POSTED BY: Pokernicus
Overall rating: 4 out of 5 4 out of 5

I've had this laptop for a few months now, and I really like it. It's got great battery life, although I probably keep the screen relatively dim, which conserves battery life. I have more to gripe about with Windows 8 than the laptop itself. My only complaint would be the keyboard; some of the keys on the bottom row get stuck. It's not horrible, but if it gets worse, I would consider utilizing my warranty. Overall though, good machine.

Good computer

POSTED BY: Freelancer , Salt Lake Utah
Overall rating: 4 out of 5 4 out of 5

I have had this computer for about three weeks. I have really enjoyed using it. It is light, and with what I use it for I get about 4-5 hours of battery life, which is good. My only complaint is that it does run a little bit warm when I use it for games, or even sometimes when I use Adobe Apps. Although this is bearable and I have not had any problems with it overheating I could see this as the only problem with this system in the foreseeable future. I highly recommend this computer because it is a powerful system in a sleek package. However, if you are going to do anything beyond basic business functioning I recommend getting a cooling pad. The one I got seems to keep the system about 10%-15% cooler. This is the second Toshiba I have owned and I would defiantly buy another one
  • $899.99
  • -$80.00
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • $
  • $819.99
  • »
  • Free Ground Shipping

add to cart
  • Laptop summary This product is prebuilt.
  • Intel® Core™ i5-4200U processor
  • Windows 8
  • 8GB DDR3L memory
  • 1TB (5400RPM) hard drive with 32GB solid state disk cache
  • 1366x768 TruBrite Touchscreen display
  • Mobile Intel® graphics
  • Intel® Wireless-N 7260, 2x2 BGN + Bluetooth 4.0 (Wi Di ready)
  • Premium Raised Tile Keyboard
  • Integrated HD webcam
  • Starting at 4.6 lbs
  • Accessories Added: