Toshiba Satellite E45T-B4204 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

My Review

POSTED BY: airbusking , San Antonio TX
Overall rating: 5 out of 5 5 out of 5

I selected the Toshiba B2404 over a Mac Pro, I own several Mac (iMac, iPad, iPhone ... ) products but after careful review I chose to go with Toshiba. Value was my primary concern, however, I am very impressed with the quality, I was not out to get a touch screen but I am glad that I did .... I love it! Overall I am impressed!

Great little machine!

POSTED BY: Happy Camper! , Dalzell, SC
Overall rating: 5 out of 5 5 out of 5

I love everything about this laptop -- even the feel of the keyboard! It's a nice size -- not too big or heavy to travel with and it has a quick response. Love it!

Great laptop - difficult setup

POSTED BY: HR lady , NC
Overall rating: 5 out of 5 5 out of 5

Love the laptop and value, very difficult to almost impossible to find manual to help with initial setup and understanding. Some of us like to read and understand before launching. Should get mailed to you, or be available by link at time of purchase.

Nice laptop

POSTED BY: Farmlady , Yale MI
Overall rating: 5 out of 5 5 out of 5

This new laptop is really nice to use. Love the key backlights. Light weight and battery power really goes a long time without being plugged in

Excellent laptop

POSTED BY: chairman of the board , Monmouth, ME
Overall rating: 5 out of 5 5 out of 5

This is the 3rd Toshiba laptop I have owned. I have found them to be trouble free and reliable.

happy to have this laptop

POSTED BY: Doc , Manila, Philippines
Overall rating: 5 out of 5 5 out of 5

Very clear high definition quality 14 inch wide multi touch screen. Illuminated keypads for use in dim situations like airplanes. Very light in weight. Slim design sleek.

PC Replacement

POSTED BY: MikeM , Richmond, VA
Overall rating: 5 out of 5 5 out of 5

I bought this laptop to replace my home pc and it is just perfect for the job. I added my old 21" monitor and wireless mouse and keyboard and now I have a new up to date computer that can go with me if needed. If I want to use the touchscreen, I just open it and touch away.

Nice laptop

POSTED BY: Dan , Elgin, Il.
Overall rating: 5 out of 5 5 out of 5

I had 3 Sony laptops before this and the first two were real good. The last one was not so much. This Toshiba has been real good so far. I have had it one month. No complaints at all.

Toshiba Satellite 14" i5

POSTED BY: Brian , Littleton, CO
Overall rating: 5 out of 5 5 out of 5

Excellent laptop. Going from an older 15.9" Satellite to this 14" has been huge. The difference in size and weight are fantastic. The i5 processor is extremely fast. Reboot takes less than a minute.

POSTED BY: chica01 , Sound Beach, NY
Overall rating: 5 out of 5 5 out of 5

Very Good Laptop love to work

POSTED BY: Mathai , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

I love Toshiba Satellite E45t because of lightweight, nice design and look and finally high resolution touch screen.

My First laptop and First Toshiba

POSTED BY: Honda Guy , Decorah.IA
Overall rating: 4 out of 5 4 out of 5

I see this laptop as having both Pro's And Con's. Pro's Very easy to use Keyboard; Very Clear Screen; Touch Screen Capability; Laptop Size Is Perfect For My Needs. Con's: Minimal Warranty Of Just 1 Year.; Pricey Extended Warranty Contract;No Instruction Booklet.

Good laptop

POSTED BY: Andy , Seaford ,NY
Overall rating: 4 out of 5 4 out of 5

One failure---one USB port fails to function.

Great Bang for your Buck!

POSTED BY: Jake , NC
Overall rating: 4 out of 5 4 out of 5

This laptop provides very good performance in a small, cheap package. The screen resolution and contrast is great! Very nice, user friendly features and quick loading. Windows 8 can make the system lag a bit, but I would reccomend the computer!

Great Laptop

POSTED BY: Oscar , NOLA
Overall rating: 4 out of 5 4 out of 5

The laptop is fast and easy to use. The keyboard is comfortable and easy to navigate. Windows 8, however, is horrid!

This laptop is just right

POSTED BY: NewToshgirl , Greenville, SC
Overall rating: 4 out of 5 4 out of 5

This laptop looks beautiful. The metal finish seems to help keep the laptop cool. But I haven't had any problems with overheating, and I work on Adobe photoshop and look at internet videos at the same time. It is not too sluggish while opening multiple programs. The start-up time is super fast. I do not have to wait for the laptop to load up at all. The keyboard has a nice feel to it. I love the keyboard. I love the way the keys make a clicking sound as I type. The keys are spaced out properly so you don't make as many mistakes. I don't really use the keyboard light. But it is there if I need it. I'm glad there is an option to turn it off so that I can save some battery. The touchscreen is very responsive and not too sensitive. But it does leave a lot of fingerprints which is unavoidable with any touchscreen. The sound is pretty nice, almost stereo-like. It gets really loud and does not have too much treble. It helps when watching videos with low sound. This laptop is very light. Since there is no disc drive it's like carrying a medium sized paperback 500 page book. I think the battery life is decent. I can get about 3-4 hours out of it before I have to plug it in. I love this laptop. the only problem I have is with the mousepad. Overtime it seems as if the left side gets overused and the mousepad becomes unbalanced. The left bottom corner gets pressed into the laptop so overtime you may have to push harder to click. The top left corner has become raised as a result of pushing the left click so much.

feature rich, some quirky performance

POSTED BY: bklyn , New York, ny
Overall rating: 4 out of 5 4 out of 5

overall this product has performed as expected. the battery life is just average and a couple of features (glide pad and others) didn't seem to work correctly. after finally getting a human being to answer our service call we have been able to resolve both issues with the first call

Great product for the money!

POSTED BY: SusanG
Overall rating: 4 out of 5 4 out of 5

Great laptop for the money! Love the ease of use and all of this laptop's features. Just wish I got a little more battery life.

Love the laptop - but....

POSTED BY: Jon , West Palm Beach, FL
Overall rating: 3 out of 5 3 out of 5

Please bear in mind that I have been an AVID Microsoft evangelist for almost 30 years. All the computers in my house are Toshiba laptops with the exception of one work machine, so I am biased (admittedly). The laptop itself is a fine performer, but since i am in deep hate with the operating system and I have no real way of backing up my OS (no optical drive - no recovery media/medium) I am hesitant to move away from the absolutely terrible Windows 8. I am in the process of evaluating Windows 10 on my other machine(s) and if this proves viable, I will upgrade this machine. Shame, I like the laptop fair enough but because of the bad OS experience, the machine sits in a corner - barely used

Good laptop

POSTED BY: Abdul Khader , Ajman, UAE
Overall rating: 3 out of 5 3 out of 5

It's overall a good laptop. It would be nice to see dvd drive buit-in.

Good concept bad parts and assembly

POSTED BY: Azlid131 , Sherman Oaks CA
Overall rating: 2 out of 5 2 out of 5

Do not buy!

No Drive

POSTED BY: t , Philadelphia, PA
Overall rating: 2 out of 5 2 out of 5

I am disappointed that the laptop does not come with a standard CD/DVD drive. I'm also disappointed in the new Microsoft operating system. The laptop performs well and I like the touch screen capability. I am a loyal customer of the Toshiba brand but am disappointed in this purchase.

unsatisfied

POSTED BY: yahia , Egypt
Overall rating: 2 out of 5 2 out of 5

I have a lot of negative signs, for example: Feeling static charge during battery charging. the voice that heard during using mouse pad Microsoft office not installed only one partition C, where I can save my data. All the above from using this lap just twice !!!!!

Not very Happy

POSTED BY: b2mj44 , Wisconsin
Overall rating: 2 out of 5 2 out of 5

The keys are suppose to be back lite and they are not. Hate the tough screen. and the system will start to flash on and off when it wants. very poor for the cost

MSRP: $811.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-4210U processor
  • Windows 8.1
  • 6GB DDR3L 1600MHz, (16GB Max, not user upgradeable)
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • Sold Separately: DVD-SuperMulti drive (+/-R double layer)

shop for accessories