Satellite L305-S5917

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»


POSTED BY: Cag , Dallas
Overall rating: 5 out of 5 5 out of 5

Bought this in January and never a minute's problem with it. Couldn't be happier and highly recommend all things Toshiba. (Goodbye, Dell!)

My first ever Toshiba laptop, and I love it

Overall rating: 4 out of 5 4 out of 5

I really enjoy using this. It's easy and quick!

Ugh, Don't get me started on this....

Overall rating: 1 out of 5 1 out of 5

I had nothin' but problems with my Satellite L305-S5917... I had my computer repaired once, and then within the followin' 2 to 3 weeks I had the same exact problem, (which the first time was my boot sectors were faulty, and need to have a brand new hard drive put in)... And now I have the same problem...I really don't like this laptop...

MSRP: $417.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Celeron® Processor 585
  • Windows Vista® Home Basic (SP1, 32-bit)
  • 1GB PC6400 DDR2 800MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories