Satellite L305-S5929

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

satellite l305 series

POSTED BY: msw , mckinleyville,ca
Overall rating: 5 out of 5 5 out of 5

have not used much because of limited wireless range. amd battery life ,i would appreciate if you coud tell me how to increase wireles range. this is a update to a survey exactly the same. i do not wish to really review at this time,have not used long enough,but my neighbor received a product for less . it it seems to have beter wireles range

Decent Laptop

POSTED BY: A.Andrew , Carribean Sea
Overall rating: 4 out of 5 4 out of 5

This is probably one of the best laptops you can get for the money with 2GbRAM and A 250GB harddrive. If it had 4G Ram and Blue Tooth I would have given it five Stars. The speakers are poor quality, but what can you expect for the price you can't go wrong.

satellite l305 series

POSTED BY: msw , mckinleyville,ca
Overall rating: 3 out of 5 3 out of 5

it is a good computer.i do not beleive,i shoud really comment about it. it is a avereage computer so far. battery life is poor,i think the battery is the only problem i have right now and the range you can pick up wifi signal. if there was a way to increase the wifi signal tell me.i can not even get the wireless signal to reach garage,not far at all.

MSRP: $549.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T3400
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories