Satellite L305-S5941

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

My Toshiba

POSTED BY: Rave18 , Tacoma, WA
Overall rating: 5 out of 5 5 out of 5

When i first got my toshiba i was very excited to go home and use it. so i got home and opened it up and was amazed by the graphis and how good it was running. if i were to recommend any laptop brand it would for sure be a toshiba.

Not too bad

POSTED BY: Sieve33 , Boston MA
Overall rating: 4 out of 5 4 out of 5

I am pleasantly surprised with this laptop. it has all the features I wanted and the low price I needed. the only lacking point is the battery life, but since I know the life of the batteries, I can plan for that. It takes a little longer than expected to boot up, but I can live with that also.

Efficient for college, work, etc...

POSTED BY: Laura , Lufkin, Texas
Overall rating: 4 out of 5 4 out of 5

I only have a few complaints. A few of my keys will randomly start typing without me even touching them. I have no clue why. I use my laptop a lot. It has been a blessing for doing my college work. I really enjoy being able to carry something that's not to heavy. I'm a forestry student and I have several nice programs and software packages that I use for Geographic Information Systems. This laptop supports the software needs. I've not run into any problems with this laptop other than the keys going crazy. I wish it came in another color, but I settled for the great price and its features.

MSRP: $568.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor T6400
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 3GB PC6400 DDR2 800MHz SDRAM
  • 200GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories