Satellite L305-S5942

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Satellite® L305-S5942 - Great Buy great Prics

POSTED BY: Gawain , Kingston, Jamaica
Overall rating: 4 out of 5 4 out of 5

Its a great product. It handles basic operations well. Great laptop to start off with.

Great for the price

POSTED BY: Qman , Roseville, California
Overall rating: 4 out of 5 4 out of 5

Someone told me to look at a Toshiba when I was considering a laptop. I have used Dell and IBM laptops in the past. I am very pleased with the features and value.

"WOW"

POSTED BY: reggie
Overall rating: 4 out of 5 4 out of 5

I really like this laptop.The battery life is not as long as I would like for it to be,but it will have to do for now.But for the price I would recommend this laptop to anyone who needs one.

So far so good

POSTED BY: Lextec
Overall rating: 4 out of 5 4 out of 5

I don't understand why the window's operating systems disc did come with the laptop. First time I've ever purchased a system with installed software and the original disc were not supplied with the product. I would really like an explanation for this. Product has operated flawlessly since purchase.

MSRP: $749.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor P7450
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories