Satellite L305-S5948

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

A Very Good Laptop

POSTED BY: LazyAce , Las Vegas,NV
Overall rating: 5 out of 5 5 out of 5

This is a very good Laptop and it is very reasonabley priced. I like the built in Webcam and mic

awesome

POSTED BY: Naomi , Berkeley, CA
Overall rating: 5 out of 5 5 out of 5

i love this toshiba and i had one before, but honestly, i hated that one and the battery was horrible so I told myself that I would never get a toshiba again, but this one totally exceeded and surpassed my expectations

terrific buy

POSTED BY: Didi , Houston, TX
Overall rating: 5 out of 5 5 out of 5

I am thoroughly enjoying my new laptop. I had actually bought my husband one for his birthday and he uses it all the time, I did not need as much storage space, so I opted for this model. I also bought one for my sister the same day.

totally satisfactory

POSTED BY: dodge , anaheim,ca
Overall rating: 5 out of 5 5 out of 5

I purchased my laptop about 2 months ago and had not really tested it to the extreme. I have now had it on the road in China for about 3 weeks and am totally pleased with it. Several times I have been without power for a couple of hours and never known it the battery is so good. Also my boss has had to on occaion use my laptop because it seems to always keep running in a pinch. Very good product.

Great Laptop for the review

POSTED BY: Melchor , Phoenix, AZ
Overall rating: 5 out of 5 5 out of 5

For the price, it serves the purpose as a secondary laptop for accessing the internet. It is very easy to use. The only complaint that I have is that the battery life is a little short.

Hugely Impressed

POSTED BY: Hawkeye , Winchelsea U.K.
Overall rating: 5 out of 5 5 out of 5

I am totally delighted with the performance, light weight carrier, easy to command and general compacability of my Toshiba

Our first laptop

POSTED BY: pvdbeek
Overall rating: 4 out of 5 4 out of 5

We are very happy with our new Toshiba laptop. Now we can travel and still easily check our email.

one great Laptop

POSTED BY: X , san diego, ca
Overall rating: 4 out of 5 4 out of 5

This is my first Toshiba. I was very impressed with the light weight and sleek design. This unit is just righ for me. Even though I have large hands the Laptop is very responsive.I picked up this Laptop and i've barely put it down. I use it more than I use my PC.

MSRP: $444.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Celeron® Processor 585
  • Windows Vista® Home Basic (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 200GB HDD (4200rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories