Satellite L305D-S5914

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

GREAT VALUE

POSTED BY: BILLYBOB , OREGON
Overall rating: 5 out of 5 5 out of 5

I PURCHASED ONE OF THESE AND I FOUND THE DISPLAY TO BE VERY CLEAR AND BRIGHT. THE INTERNET TRANSFER RATES WERE QUICK. HIGHLY RECOMMENDED AS A GREAT VALUE FOR A MID-LINE COMPUTER

my first laptop

POSTED BY: dj dave , san antonio,texas
Overall rating: 5 out of 5 5 out of 5

as laptops go i guess i'm satisffied in the satelite's basic usages. and ease of opperations. although i am not a big fan of windows vista, the vibrant colors in this display screen is awsome. i have purchased an external mouse only because i'm not proficient with the finger pointer. the pointer is too sensitive for my heavy fingers. if i had the choice i would have opted for a tilting keybord.and more data access ports. non the less, that option can be picked up as an accessory. overall i am completely elated with my purchase of the satelite L305D and would reccomend it to anyone looking for performace for value. thanks Toshiba

My New Lapton

POSTED BY: kay , tennessee
Overall rating: 5 out of 5 5 out of 5

this is the first laptop I have owned and I love it. the convencience of not having to sit at my desk is great. to be able to have intenet anywhere in my home is great!!!!!

Good Buy

POSTED BY: Bob , Indiana
Overall rating: 5 out of 5 5 out of 5

The best buy for the money. It has usb connections and easy to get on line.

First Laptop I've Owned

POSTED BY: mt , Marietta, GA
Overall rating: 4 out of 5 4 out of 5

I'm very pleased with my laptop. It's my first one and I must say it fulfills all my requests.

Nice

POSTED BY: Migz , Mountain View, CA
Overall rating: 4 out of 5 4 out of 5

This Laptop is nice. For a nice price I never imagined that I can actually get a fair game for buying this laptop.

good laptop but!

POSTED BY: larry , kissimmee,florida
Overall rating: 3 out of 5 3 out of 5

third toshiba laptop in 3 years all 3 dvd doors will not work properly

Frustrated

POSTED BY: Frustrated , Goodyear, AZ
Overall rating: 2 out of 5 2 out of 5

I've owned the laptop less than two months and it's in the shop already!! Not quite what I was hoping for in terms of reliability...

MSRP: $419.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Sempron™ 3600+ processor
  • Windows Vista® Home Basic (SP1, 32-bit)
  • 2GB PC5300 DDR2 667MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories