Satellite L305D-S5930

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Good Value

POSTED BY: Nick , Sacramento, CA
Overall rating: 5 out of 5 5 out of 5

I have own a Toshiba Satellite in the past, and was happy with it. This is why I purchase another one. I have had it a couple of months, and seems to be just as good. It was a purchase for my son for graduation, so I was also looking at gamming capabilities. It works fine with games like "Far Cry" which has very good graphics. Overall a very good value.

Best Laptop I've ever had!

POSTED BY: Maggie , Arlington, TX
Overall rating: 5 out of 5 5 out of 5

Great, Words can't describe all I can do with my new Toshiba L305D-S5930. Love the Photo Gallery. New games for me, too. Best of all I work much better in my business since I've had this laptop. THANK YOU,.

Excellent value laptop

POSTED BY: Pops , Conroe, Texas
Overall rating: 5 out of 5 5 out of 5

This is a laptop that I bought to use at home and on the go after retiring, the laptops that were used by the company were Panasonic and Dell, and both had problems with the programs being used and keeping data, they were also bulkier and heavier. This unit was cheaper and has a better working capacity in a slimmer body, and has been able to handle without flaws the same programs the others could not.

POSTED BY: XX
Overall rating: 5 out of 5 5 out of 5

One way that this laptop could be better is to include a schematic when the laptop is purchased. I really need this and can't find one on your website or the internet.

Not too shabby

POSTED BY: Downtown , Benicia, CA
Overall rating: 5 out of 5 5 out of 5

Seems to do what I want. Serves my needs.

Great Bang for Buck!

POSTED BY: Zoombeezie , Portland, OR
Overall rating: 5 out of 5 5 out of 5

This laptop gives you everything you need for cruising the internet to playing games!

Great value

POSTED BY: Chuck , San Jose
Overall rating: 4 out of 5 4 out of 5

The Toshiba L305D is providing very good value. The product is stable and performance is fine. Features are good. Only drawback: Would prefer USB and power connectors on the rear to avoid cables on the side. Overall, I would recommend.

Very pleased

POSTED BY: jer , OR
Overall rating: 4 out of 5 4 out of 5

A great laptop I can take worry-free overseas. Would love it a bit smaller with more battery, but I chose the large screen and you CANNOT beat the price and quality!

Good Value for Price

POSTED BY: michaelhb1 , Phoenix, AZ
Overall rating: 4 out of 5 4 out of 5

Overall it's a good laptop for my purposes, i.e. traveling, internet, e-mail etc. The battery life is quite low (maybe 60-90 min.) and i'm not very happy with the VISTA Home Prem. operating system, it's very slow and bogs down alot,

Toshiba Sound and Vista

POSTED BY: Soundman , Vancouver, WA
Overall rating: 3 out of 5 3 out of 5

I recently purchased my Laptop to do some work and some play. The Machine is quick and has great graphics. I play my favorite vidio games on it and run AutoCAD. My only problem is This computer will not allow Audio passthrough to the speakers. This is something I have done even with the cheapest and weakest computers I have ever owned. Finding the problem. The Realtek Audio either does not allow or is not VISTA compliant to do this. So things such as karaoke or recording sound track with a monitor are out of the question. I had to purchase a card to do what any other computer I have ever had or used could.

MSRP: $549.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Athlon™ X2 QL-64 Processor
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 3GB PC6400 DDR2 800MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories