Satellite L305D-S5940

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: pappiya , illinois
Overall rating: 5 out of 5 5 out of 5

i give it five stars it a great laptop and yes i wll recommend it to my friends and famliy!

FAST

POSTED BY: topaz , Citrus Heights, CA
Overall rating: 5 out of 5 5 out of 5

Loving my new laptop. Much faster than my old one. Nice to bootup and be at the welcome screen immediately..

Very good lap top

POSTED BY: FGOODIE , Sun City West, AZ
Overall rating: 5 out of 5 5 out of 5

Very user friendly. Easy to set up. Excellent battery life.

Recommended

POSTED BY: mike , Tucson, AZ
Overall rating: 5 out of 5 5 out of 5

I like this laptop. The price was great and it performs very well. Powers up quickly and the screen is easy on the eyes. For me, its all I need for power and storage. The only minor point is the battery life is a bit short and the sound isn't always loud enough. NO problems otherwise.

Good buy

POSTED BY: J James , Stormville,NY
Overall rating: 5 out of 5 5 out of 5

I recently bought this computer so I wouldn't have to compete with my kids for our other computer. I wanted something efficient and reasonably priced. So far, I am very happy with this product and have had no problems.

Satellite as a school tool

POSTED BY: The Rev. , Westerm Connecticut
Overall rating: 5 out of 5 5 out of 5

Bought this for my son, his school allows Laptops in class for note taking and project work. He is happy with speed and performance but regrets the lack of a camera. I chose this model for is lack of camera, its a school tool, not a toy. Frankly, the battery is short on life, it will not get him through his normal day. I will buy another as a backup, but be ready to do the same. Seriously, it is a GREAT school tool. We are both pleased with this lappy.

1st laptop

POSTED BY: pek , san francisco
Overall rating: 5 out of 5 5 out of 5

very nice

Super Tech Support

POSTED BY: Computer Novice , Bend, OR
Overall rating: 5 out of 5 5 out of 5

Love this computer!! It is fast, easy to set up - especially with the great tech support. They are professional, friendly, courteous and most of all don't treat me like a moron - which would be easy to do as computers are not my area of expertise!! My brother recommended TOSHIBA as he has bought about 20 and said they are very reliable.

POSTED BY: jayne , Indianapolis, IN
Overall rating: 4 out of 5 4 out of 5

I have been using laptops since 1988 and this is my ninth one and my sixth toshiba. Like all the rest, this one is durable, reliable, and an excellent value.

toshiba

POSTED BY: Werner , Seattle, WA
Overall rating: 4 out of 5 4 out of 5

I like it so far.

Excellent back up laptop

POSTED BY: JP , Dallas, Texas
Overall rating: 4 out of 5 4 out of 5

Excellent laptop as a backup to my home system. Full featured, very fast, excellent graphics for home use.

Good Laptop for the money

POSTED BY: Mak , houston, tx
Overall rating: 4 out of 5 4 out of 5

Good laptop for teachers and students.

First Laptop - I LOVE IT

POSTED BY: Murph , San Diego, CA
Overall rating: 4 out of 5 4 out of 5

I had tried three laptops and didn't feel comfortable with it. I must tell you that I am 72 years old. I opened this computer and felt immediately at home.

Good beginner's Laptop at a good price.

POSTED BY: zbowdawg , Chandler, AZ
Overall rating: 4 out of 5 4 out of 5

Have had no issues since purchase. Performs better than expected for the price. Fast... good for minor gaming, internet, photo sharing and basic personal computing and just plain easy to use for my kids. I bought two and very glad I did.

Solid performance

POSTED BY: Shalework , Houston, TX
Overall rating: 4 out of 5 4 out of 5

This is my second Toshiba laptop. First one I had for two years and was stolen in a burglary. This one runs better and seems easier to use. Too bad it came with Windows Vista. At least most of the Vista problems I had with the old machine seem to have been fixed in this version. I mostly use the net and wordprocess on the machine, and it is fine on the word processing, a little slow at times for the net. Display is nice, would be nice if the ports and other connections on the sides of the mahine were also labelled on the surface of the keyboard for easy finding for portable use. Can't really rate for battery use as I generally keep it plugged in when using. Wish I had a 3.5 floppy as well as the cd-rom

So cheap and worth it.

POSTED BY: crm , Seattle, WA
Overall rating: 4 out of 5 4 out of 5

Got this laptop on an insane deal and its been worth every penny. Though the CPU runs rather hot (I prefer the more efficient Intel to the AMD), its the only thing I would change. Overall, totally satisfied and would recommend to friends/family.

Hot Laptop

POSTED BY: jcgg , Huntington Beach, Ca
Overall rating: 3 out of 5 3 out of 5

aptop runs very hot. I can fry an egg with the heat from the exhaust fan. For the price the laptop is a good deal. I can't complain I was looking for an inexpensive Wifi latop with a dual core AMD chip and that is what this laptop is. Please cool it down.

POSTED BY: g , aurora,il
Overall rating: 3 out of 5 3 out of 5

I generally like it. However the sound level is too low. There does not seem to be a way to make it loud enough.

MSRP: $483.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Athlon™ X2 QL-64 Processor
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 2GB PC6400 DDR2 800MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories