Satellite L355-S7900

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

POSTED BY: V
Overall rating: 5 out of 5 5 out of 5

A very good and solid product

Great Overall Laptop

POSTED BY: sandy , Macedon, Ny
Overall rating: 5 out of 5 5 out of 5

I never had one before so I asked a local computer store owner what he sold and he sid the only brand that keeps my customers happy. Toshiba. The features were unbeleiveable and so easy tostart using the laptop. I would buy another for my husband. I had difficulty with backing up and got on a call with Toshiba, they didn't get off until it was fixed.

size and value

POSTED BY: small business
Overall rating: 4 out of 5 4 out of 5

I purchased our laptop at a local wholesale club. I was suprised to find a laptop with a 17" monitor in this price range. Now that we have had the laptop for four days I have enjoyed the large wide screen and the quality it offers. I was not impressed with the DVD movie quality playback but it gets the job done. I am also finding that the mouse control is a challenge to operate . I t tends to jump around . My previous laptop was a Dell and I was acustom to tapping the pad to get the curser to show up in a dialogue box for eaxmple . The Toshiba requires lining the mouse curser p on the box and then clicking the left clicker to engae the typing action. It is a large laptop and since it won't leave the ooice it works for us but I would caution for ease of portability since there are many smaller ones avaialble today. If you want exceptional value, basic wordprocessing, internet use, web cam use go for it, we did!

Decent laptop for the money.

POSTED BY: Lisa
Overall rating: 4 out of 5 4 out of 5

I have only two complaints. The battery life is short and Windows Vista is not compatible (with no available fixes) with some of my software. Other than that, the system is a great buy for the money.

Very Good Laptop

POSTED BY: JJ , Georgetown, DE
Overall rating: 4 out of 5 4 out of 5

Laptop is a very good performer. User friendly. This is my second one. Would buy one again. Tech staff is the best I've ever dealt with, they are not only efficient...they are kind and respectful and thourough. For me...they are the best of Toshiba.

great size laptop

POSTED BY: ziggy , buffalo, NY
Overall rating: 4 out of 5 4 out of 5

I recently purchased a 17" Toshiba Laptop and i am very happy with the features expecially the built in camera.the only thing im dissapointed in is that i had to purchase a carry backpack on my own.

MSRP: $629.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T3400
  • Windows Vista® Home Premium (SP1, 32-bit)
  • 3GB PC6400 DDR2 800MHz SDRAM
  • 160GB HDD (5400rpm, Serial ATA)
  • DVD SuperMulti (+/-R single layer) drive
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories