Satellite L455-S5009

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop!

POSTED BY: js , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

We have had this laptop for several weeks now, and we have no complaints! Especially for the price! The speed as AMAZING! So far so good, and I would recommend this to anyone.

Meat and Potatoes System

POSTED BY: asauce99 , New Orleans, LA
Overall rating: 4 out of 5 4 out of 5

Got this laptop two weeks ago, and so far it's exactly what i was looking for. Nothing fancy...no fluff...just a hardy little system that gets the "every-day-use" jobs done. Like I said...a "Meat and Potatoes System". And the performance to price value is really great. I am very, very satisfied with the processor speed, and the memory. I have no problems running the internet....even with a weak wifi signal...it's incredibly fast. What more could you ask for for the price? A high def...nearly 16" screen...4 gigs of RAM and a 320 Gigs of hard disk space, as compared to the L455 S5008, but you get the S5009 for $10 CHEAPER! I'll pay $10 LESS for 70 EXTRA gigs of hard disk space ANY day! The only other difference between these two laptops may be in the pre-bundled software that comes with the system. Overall, I'm very pleased with this laptop. Sure...it isn't going to get any second looks right off the bat...but trust me...those who DO give it a second look, will be pretty impressed upon closer examination. Especially...once they hear the price! Nice.

better than hp

POSTED BY: nick , dallas,tx.
Overall rating: 4 out of 5 4 out of 5

this is a great lightweight laptop. one year ago i purchased an hp that cost twice the price. the toshiba stay connected wirelessy. the hp will not. this is a great laptop for the price.

Awesome Laptop

POSTED BY: Star , Ft. Lauderdale, Florida
Overall rating: 4 out of 5 4 out of 5

This is an amazing laptop, especially for the price. I was skeptical at first but so glad I purchased it. It is very fast. The battery life is about 3 hours which I wish could be more, but for my purposes it suits me just fine. I download movies and watch them with no problem and it is very fast. This computer is a very sweet deal, and I would definitely recommend it to family and friends.

Poor Quality Mouse

POSTED BY: TJH , Green bay WI
Overall rating: 1 out of 5 1 out of 5

I bought this Laptop beacuse I liked the duarbility of the keys, the price and the looks. What i missed was the VERY CHEAPLY made Mouse buttons. the Left one sticks under the surface making it impossible to use. It constantly pushes down and does not pop back up. The Right side is firm but the left is horrible!!! I would never recommend this product to anyone since I have to pick up a mouse and now cannot use the Left mouse. HORRIBLE!!!

MSRP: $539.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T4400
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 memory
  • Intel® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories