Satellite L455-S5980

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Satellite L455-5980

POSTED BY: j2mortimer , Dallas, Texas
Overall rating: 5 out of 5 5 out of 5

Excellent Machine. Easy to use, fast, very fast, even with Office 2007 Enterprise, with Visio and Communicator 2007. Windows Home Premium. Toshiba loads the machine with its own maintenance package which I have used on other Toshibas. Fabulously finds printers on networks with no IT involvement. Acquires new IP addresses without the old release/renew in DOS. Love it. I find I play with it too much. Sometimes not really getting my work done. It's actually a PC that's, dare I say it, "It's a PC that's Fun to Use!"

Great low end Laptop

POSTED BY: Jay , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

Works well out of the box with my MS Enterprise applications. Lacks video cam, mic, & HDMI output. For a 32 bit machine, it loads and runs very cool, quick, and quiet without hang ups. If windows 7 performs well long term, this machine is a winner.

very happy

POSTED BY: Katt , Floresville Tx
Overall rating: 5 out of 5 5 out of 5

when I tried your product i was very satified the the laptop feature and the beginers guides made me very happy that I had made wise choice in purchasing this product.

I Love Toshiba

POSTED BY: Barbara , Knoxville, Tn
Overall rating: 5 out of 5 5 out of 5

I now own 3 toshiba laptops and I love them! This newest one is awesome, easy to use, comfortable to use. I love the widescreen, the keyboard, everything! It didn't come choked up with too much tryware and it is fast, efficient and everything I wanted and more. Yes, I own 3 and will own 4, so every member of the family will finally have thier own!

Nice Notebook

POSTED BY: Cozone , Everett,Wa.
Overall rating: 5 out of 5 5 out of 5

This Notebook does everything i like and more, Has a Nice size screen. Plus does not get Hot like my old notebook did. Only thing i wish is they would come out with is a battery that would last longer then two hours and 45 mins. Other than that i love this Notebook so far..

Easy to read screen

POSTED BY: Mar , Englewood Florida
Overall rating: 5 out of 5 5 out of 5

Since I am a senior citizen I needed something easy to work and also easy to be able to read. I found this to be so with my new Toshiba. Thank you very much.

greatest christmas from my children

POSTED BY: mustang , Pulaski, TN
Overall rating: 5 out of 5 5 out of 5

I really like it, and it does do everything I need, (that I have found out) todate

just go it

POSTED BY: stuffman , ringgold,ga
Overall rating: 4 out of 5 4 out of 5

Well, ive had it for a week pretty good for the price. Features simple could have a little more but a great gift for someone who needs just a simple labtop that works just fine.

Good Value

POSTED BY: TheComputerShopper
Overall rating: 4 out of 5 4 out of 5

This laptop isn't exactly the best. It has a simple Intel Celeron processor, and it sounds like a terrible budget laptop. However, upon operating this, it seems very fast for a one star processor. The screen is bright and glossy, and it handles tasks very quickly. The keyboard is standard and feels sturdy and nice, and the trackpad feels like any other. One thing I do not like, however, is are the limited features. There aren't many USb ports, and no firewire. All in all, this is a quality budget laptop.

very good laptop

POSTED BY: jc , sc
Overall rating: 4 out of 5 4 out of 5

this laptop dose every thing they say it will do . the only complant i have is can not run on battry power very long aprx 30 min

Good punch for the buck

POSTED BY: Jim! , South Carolina
Overall rating: 4 out of 5 4 out of 5

Nice machine. So far, there are a few things that impress me about this computer, and they are as follows: One thing is that it boots and shuts down very fast. This may be the computer, or Windows7, but it is great knowing it will be running right away. So far, I have thrown some heavy stuff at it, like video editing and rendering, without any problems. The video is good, and does excellent for a laptop. So far, it has crashed only once, but recovered quickly. Not bad at all.

Very good laptop

POSTED BY: Mikulas , Venice,CA
Overall rating: 4 out of 5 4 out of 5

Replaced desktop

POSTED BY: texast , Ft Worth Tx
Overall rating: 4 out of 5 4 out of 5

Has worked good as a replacement for desktop with Windows XP. Windows 7 took me awhile to locate everything, but feel comfortable now. Good clear screen, nice key feel, plenty of features. Only real complaint is QUALITY of built in speakers.

Good computer

POSTED BY: roxanne , hollywood, CA
Overall rating: 4 out of 5 4 out of 5

good for price

Microsoft Office

POSTED BY: Princesire , Ft. Lauderdale, Fl
Overall rating: 3 out of 5 3 out of 5

For the price it isnt a bad laptop. The only draw back was, it is loaded with Microsoft Office and Micosoft Works but you have to buy the Micosoft Office you only have a trial verson loaded in so it will cost you an additional money. My other computers that I have brought always pre loaded with no extra cost so be aware of this.

Good Student Laptop

POSTED BY: dad , La Palma
Overall rating: 3 out of 5 3 out of 5

This laptop fully meets the needs of my Jr High School student daughter. It allows her to get her homework done (after purchasing additional software) and still stay in touch with her social network. I'd recommend this for users who are not too demanding on speed/power.

MSRP: $449.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Celeron® Processor T3000
  • Windows 7 Home Premium (32-bit)
  • 2GB DDR2 800MHz memory
  • 250GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Realtek 802.11b/g wireless-LAN

shop for accessories