Toshiba Satellite L55-A5226 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

High Tech and challenging

POSTED BY: Yahwing , Stephens City, VA
Overall rating: 5 out of 5 5 out of 5

The Toshiba Satellite L55-A5226 laptop is geared more for the technical savvy. I love my laptop but find it challenging to maneuver through all the applications. I thought it was me, however, my husband who is tech savvy found it difficult to use as well.

Satalite L55-A5226

POSTED BY: ljkats , Austin, TX
Overall rating: 5 out of 5 5 out of 5

My 2nd Toshiba home laptop in 6 years.. probably won't ever consider any other brand... have used many brands at work and tell everyone my laptop at home is much better

Good Laptop

POSTED BY: Damian , Hartford,CT
Overall rating: 4 out of 5 4 out of 5

This is a good laptop for games like Counter Strike. It runs CS very smoothly and the graphics are good. The battery at full charge says 5 hours and the laptop hasn't gotten hot while I have been using it. Very good laptop because it wont lag you out of programs, the college student would be very pleased with this as would a semi avid PC gamer.

Brightness

POSTED BY: May , Virginia
Overall rating: 4 out of 5 4 out of 5

It's a good computer but the only thing that's wrong with it is that the brightness buttons don't work and the panel where it allows you to drag the bar for how high or low you want the brightness to work doesn't work either and it's a brand new computer.

TOSHIBA SATELLITE L55-A5226

POSTED BY: GLO
Overall rating: 4 out of 5 4 out of 5

I REALLY LIKE THE EASE OF USING WINDOWS 8, LOVE THE KEYBORD.

Clickpad location

POSTED BY: Terson , montreal quebec
Overall rating: 4 out of 5 4 out of 5

The only disappointment is the fact that the clickpad is not centrally located. This is in my opinion a poor design and has the user constantly having to adjust positions to be able to activate the clickpad properly.It would be better if they relocate the clickpad to provide the end user with an easier and less frustrating experience.

Good Laptop for work

POSTED BY: Gcroci , Montevideo, Uruguay
Overall rating: 4 out of 5 4 out of 5

It is a good laptop for work. Only improvement, install bluetooth.

i like it

POSTED BY: snakecharmer
Overall rating: 3 out of 5 3 out of 5

yall need to make windows as easy as vesta or xp was older people cant work windows 8

laptop

POSTED BY: pj , Warner robins ga
Overall rating: 2 out of 5 2 out of 5

Really like the laptop but am extremely disappointed that after two weeks of use a key fell off. I use it every day for school and cannot stop work to get it replaced until the semester is over

disappointed

POSTED BY: al , fl
Overall rating: 1 out of 5 1 out of 5

Very disappointed with this Toshiba running Windows 8. Have owned this laptop for 2 months and can not use it while with my customers because the performance would make me look like an idiot. I am still unable to do basic functions. Ready to put it on ebay.

MSRP: $603.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3337U Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L50 shop for accessories