Toshiba Satellite L55-A5284 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

first laptop scores

POSTED BY: ohiowriter , Columbus, OH
Overall rating: 5 out of 5 5 out of 5

Yeah, can you believe it? My first laptop. Feel like I need training wheels. This unit is very good, quiet, doesn't heat up much. The only complaints I do have are I don't like Windows 8 and I think I ordered too large a screen to use when I'm on the plane, which I am almost every month. Could have saved $50 or so and gotten a 14 in screen. But this is nice, big and clear. also got this computer because it has just about every input and output I could want. Gonna use it as a portable recording studio on the road next month. Overall, so far, great value.

Wise Purchase

POSTED BY: howdybub , Mt. Home, AR
Overall rating: 5 out of 5 5 out of 5

So far this seems to be the right computer for me. It is everything I hoped it would be. Only problems were man made by me. The lap top has been flawless.

Great value

POSTED BY: hwlnwulf , NC
Overall rating: 5 out of 5 5 out of 5

So far I've been quite pleased with this laptop.The performance is good and it was an easy transition to Windows 8.1. It does everything I need and the Toshiba help software answered any questions I had to get used to it.

excellent machine

POSTED BY: rossicane brazil , Piracicaba, SP - Brazil
Overall rating: 5 out of 5 5 out of 5

I think this computer is the best I have ever have. It works fast, good performance, good battery life and has a good price compared to the market.

Best Laptop Ever

POSTED BY: CarolinaGirl , Orangeburg, SC
Overall rating: 5 out of 5 5 out of 5

Slick keyboard, easy to handle, easy to understand, it's outstanding, I Love it

Excellent Value

POSTED BY: Pete
Overall rating: 5 out of 5 5 out of 5

Get it!

Love the speed

POSTED BY: Baron , Spring Hill FL
Overall rating: 5 out of 5 5 out of 5

The battery life is good. The speed is awesome. It does not generate a lot of heat, I can sit it on my lap to use it for extended periods of time without any problem. It is light weight and very portable. One irritant is the keyboard touch. It is significantly stiffer than my old machine (not a Toshiba) and I find many keystrokes not being recorded. Maybe I will adjust to this.

Nice laptop

POSTED BY: Basibob , Belcamp, md
Overall rating: 5 out of 5 5 out of 5

Good unit, not too heavy, battery. Life could be better, but screen s awesome!

Awesome Touch Screen

POSTED BY: Cinderella , Salisbury, NC
Overall rating: 5 out of 5 5 out of 5

I love the touch screen feature along with the keyboard. This is my first laptop and I am loving it. The keyboard is easy to use also. I am very pleased with this purchase so far. It has been easy for me to figure out and use. It is going to be great for my business and personal use. I like the features on the start page, especially the weather and health and fitness information.

No Stereo Input !!!

POSTED BY: Alex Prm
Overall rating: 4 out of 5 4 out of 5

Nice Lap top , everything is great , is responsive including the touch screen , but if in any time you will try to save yor record library stay away from it ,in my old HP computer I was able to record some cassettes and Lp s that i have in my library in stereo without any interface , just connecting the tape out of my receiver to the line in/mic input and presto! i had stereo signal straight in to audacity , it seems that this has been an issue with all the TOSHIBA laptops , unfortunately I can not return it , next time i will do more research , and buy an external capturer.

Great Laptop & Great Value

POSTED BY: Ordinary Average User , NY
Overall rating: 4 out of 5 4 out of 5

This laptop is light, runs fast, and is easy to use. It runs quietly and the fan is barely audible when it's running. Screen has bright, clean images and sound is good, with high enough volume for entertainment. Raised keyboard is well-spaced with large print on the keys, making them even easier to see and while there is no backlight, it's unnecessary. Great to have the 10-key on the side. Caps & Num locks have small lights on them when in use. Touchpad is no trouble, but I use a wireless mouse and still have 2 USB ports to spare, as well as several others (HDMI, network, SD, 15-pin RGB Monitor) that are helpful for everything.

Laptop Disappoints

POSTED BY: Mr. Long Island , Long Island NY
Overall rating: 4 out of 5 4 out of 5

I bought my Toshiba Laptop sight unseen because I had so much success with the Toshiba laptop I bought three years ago. It has taken me sometime to get used to the new laptop. The "mouse buttons" are much harder to use than the buttons on my previous laptop.

new to using laptop

POSTED BY: mag , ct
Overall rating: 4 out of 5 4 out of 5

only been using computer for about 1 month. only issue has been battery life.

laptop

POSTED BY: junebug , AL
Overall rating: 4 out of 5 4 out of 5

I think the laptop will be fine. My concern is that there are pre-loaded software items, along with anit-virus that I really can't use unless purchased. I would rather not have them. I'm trying to figure out how to delete them completely. I liked the days when "pre-loaded" needed software was already installed for use at purchase with no extra charge.

Almost perfect but one nagging issue

POSTED BY: skywatcher , Tampa, FL
Overall rating: 4 out of 5 4 out of 5

This laptop is sleek and much lighter than my old Dell 14" laptop. It never seems to get "hot", either. Keyboard is nice to use except that the Function keys must be used in conjunction with Fn key. I would have reversed that where screen brightness control, etc., should be used with the Fn key. One nagging problem is the touchpad. It's too wide and too sensitive. It's almost impossible to type without accidentally "touching" the area. It is not indented, either, and it's so prone to unintende touching, which causes havoc with some minor but still irritating problems.

Great Laptop

POSTED BY: Cindy , Cooperstown, PA
Overall rating: 4 out of 5 4 out of 5

I have had this laptop for awhile now and I have totally enjoyed working with it and using it for my personal work. It has wonderful features and connects easily to whatever extra things I need....USB ports, printers, copiers, etc. Great laptop to use!!!

Seems fine

POSTED BY: little john , Boulder Colorado
Overall rating: 3 out of 5 3 out of 5

Do like the size. Don't like windows 8

Humm I must have heavy fingers

POSTED BY: Mom
Overall rating: 3 out of 5 3 out of 5

My new laptop seems to react so quickly to my finger on the mouse pad. I barely touch it and the page flicks or changes with out I wanting it to. I have searched for the settings, but I am getting better at barely touching it, but its frustrating trying to not open something and it does. So if you are going through emails and you happen to go across one and it opens with out you wanting it to..... you have to ask what if that email had a virus it happens so quick. I don't really like this lap top. The right and left keys are not easy to push as they are a part of the whole mouse pad and you have to push hard just to get a reaction feels like it will break.

Not a fan... :(

POSTED BY: Iviaroko
Overall rating: 3 out of 5 3 out of 5

I wanted a Gamming Laptop, and. I knew the graphics card was not good, but I thought it could be changed. :( sad story. Knew that very late, after contacting technical support. I'm planning on selling it and get another laptop with a better graphics card. Aside from that is a very good laptop, good for business and media editing.

Poor Execution

POSTED BY: I didn't click that , Cincinnati, OH
Overall rating: 2 out of 5 2 out of 5

The trackpad is at the same time oversensitive and numb. You're constantly opening stuff you didn't mean to open. It is an absolute nightmare. Adjusting sensitivity doesn't seem to work. The battery is non-removable, yet it has the same problems with needing to reset power that all laptops have. It's not clear at all how to do that when you can't remove the battery. Toshiba seems to forget they make laptops with batteries that cannot be removed. There's no place to go for a procedure there. I defy you to find it. Toshiba installs lots and lots of bloatware. It's constantly hassling you to update it.

Should Have Never Been Made Without a Touchscreen

POSTED BY: godsblackpawn , Tecumseh, OK
Overall rating: 2 out of 5 2 out of 5

The mouse pad is way too sensitive. I believe this is due to the new operating systems for windows is set for touchscreen mode and not for a mouse pad. Thus, when you use the mouse pad, it is an utter nightmare. You open up everything you don't wish to open and you close items you don't mean to close. It is to say the least, frustrating and annoying. I hope the keyboard survives my constant pounding(which it has for 3 months, so I would say it is a durable product). As for the rest of the computer, it works fine. I blame myself, partially, for not doing more research. I didn't realize the transfer between touch screen and mouse pads was so dramatic. I had the option to purchase a touch screen for $100 more and didn't choose it, and have regretted that choice ever since. When I brought the computer home, the mouse pad seemed good for the first week, but it just kept getting worse as time went on. If you are looking at this computer, I would say, if you get the one with the touch screen, I bet it works great. But without the touchscreen, buyer beware, it is a nightmare.

Poor design and functionality

POSTED BY: Keonaona , Lodi, CA
Overall rating: 2 out of 5 2 out of 5

All Mouse pads have their issues but this one is extremely poor. The sensitivity is all messed up and sometimes just does not work at all. I had to purchase a wireless mouse and carry it with me. Key pad is also a problem. Letter keys have been sticking from day one. Certain letters may or may not work when typed. Toshiba sacrificed quite a bit in their attempt to give a sleek design. The battery life is the worst I have ever seen, it is almost as if you are recharging the old lead acid batteries that takes 8 hours to charge for 1 hour of use.

owner of a terrible laptop

POSTED BY: owner of a terrible laptop , San diego, CA
Overall rating: 1 out of 5 1 out of 5

completely dissatified.

laptop

POSTED BY: sgf , ca
Overall rating: 1 out of 5 1 out of 5

I have a laptop running windows 8 and I think the windows 8 operating system stinks, I am thinking about taking the laptop back. It will not download my HP printer software and other problems.

All's well EXCEPT...

POSTED BY: Unhappy Camper , Tampa, FL
Overall rating: 1 out of 5 1 out of 5

This is an otherwise excellent value laptop, but one thing just kills me and I'm so frustrated with it that I have to give it a 1 Star rating. The touchpad is absolutely horrendous! It is not recessed at all and it's impossible to type without unintentionally touching its surface. Barely touching it while typing sometimes shifts the cursor to a completely unexpected place. Imagine you're typing a bunch of text and suddenly you realize your text is inserted in the middle of previous text, somewhere! I downloaded and installed the latest Synaptic driver, etc., but it doesn't make any difference. I don't know why, but it seems that I experience this problem more frequently while I'm on Microsoft Outlook or Word, etc., than on a web browser. Bottom line, I'm very, very unhappy with this purchase. I had thought better of Toshiba laptops before, but not any more.

MSRP: $699.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3337U Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L50 shop for accessories