Toshiba Satellite L55-A5299 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best laptop for price dont pass up!!

POSTED BY: PuppySky , Godfrey, IL
Overall rating: 5 out of 5 5 out of 5

I was looking for a laptop that would be good through college and afterwards hopefully and this bad boy is so fast with every you do you'll truly forget you're using a laptop. I really have no idea why the price is what it is with the cpu being pretty much the best there is for laptops. the battery life is also why understated. I've had it last 6-7 hours. Don't pass this deal. I love it <3

value for money

POSTED BY: bujji , chennai, India
Overall rating: 5 out of 5 5 out of 5

I would highly recommend this product to everyone. Has one of the best processing power but missed a high end graphics card. The laptop start with high speed, got a great display and ram memory. Looks great and feels good to use.

First Laptop

POSTED BY: bob , Michigan
Overall rating: 5 out of 5 5 out of 5

I was used to desktop. Was not sure I would like the keyboard but getting used to it. Had problem with Windows 8 and mouse pad. Purchased wireless mouse and keyboard. Made the laptop a 1000% better. Still have not needed to use wireless keyboard as mostly using spreadsheet currently. It I had a paper to write or lots of text would go to wireless keyboard just because of my 40 years of type with that type of keyboard.

Good laptop, Windows 8 NO good

POSTED BY: Windows 8 hater , Dalles, TX
Overall rating: 4 out of 5 4 out of 5

The title says it all! The computer does exactly what I want, but Windows 8 needs to let me install some of my old programs rather than having to make me spend more money on updated software. I need someone to tell me how to un install 8 and load 7 onto this laptop!

Good Laptop

POSTED BY: Ray , Westminster, CA
Overall rating: 4 out of 5 4 out of 5

This laptop works really great, it is fast and powerful. The only thing that bothers me about it is the keyboard. Sometimes you have to press a key two or three times before your character is actually displayed. Not sure why this is so, other than that a very good lightweight laptop.

So good

POSTED BY: tony , CA
Overall rating: 4 out of 5 4 out of 5

I am happy with the PC, just I do not like the touch pad

Outstanding Touchpad FAIL!

POSTED BY: Jaye , Atlanta GA
Overall rating: 1 out of 5 1 out of 5

The touchpad is simply HOORRIBLEE! Seriously its a hardware fail and I am sure it's not an isolated case.

MSRP: $724.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8
  • 8GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L50 shop for accessories