Toshiba Satellite L55T-A5232 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

falling in love

POSTED BY: Girlgadget , Chicago
Overall rating: 5 out of 5 5 out of 5

I purchased the L55t-A5232, which I believe is only sold at Sams Club. This is the largest laptop I have ever had, I usually go for 13inch, but I'm not complaining. The screen is large and crisp like a 240HZ Hd tv. I love being able to charge my Iphone on it even when its off. The best feature of all is its quick startup. I noticed no difference from initial startup time , and startup after I added apps.

Great Value

POSTED BY: Binny , Fort Lauderdale
Overall rating: 5 out of 5 5 out of 5

Outstanding features for the busy road warrior small business user. This is the fourth Toshiba laptop i've had and they are consistently reliable and full featured.

Worst laptop ever!

POSTED BY: unsatisfiedcustomer
Overall rating: 1 out of 5 1 out of 5

This computer was rated highly and i loved it for the week i got to use it. i had it actually less than a week and only used it a few times. I pick it up to use it one day and the whole screen is black! The screen won't turn on and i haven't even had it a week. I am a college student and having a good laptop is extremely important. Cannot believe I spent this much money on something so unreliable.

caution!!!!!!!!!

POSTED BY: nana30 , Hiram ga
Overall rating: 1 out of 5 1 out of 5

This model has a hardware issue. I have only owned mine for 3 months having to send it in for repairs. screen goes black as if it is trying to keep from burning up. Now it has no power at all. know someone who had another model did the same thing.lesson learned

Garbage of all laptops!

POSTED BY: toshibaneveragain , Avondale, AZ
Overall rating: 1 out of 5 1 out of 5

Less than 24hrs of opening it and the screen doesn't work. Never will I buy a Toshiba! Garbage!

MSRP: $929.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-4700MQ Processor
  • Windows 8
  • 8GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L50 shop for accessories