Toshiba Satellite L55t-A5290 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

So much fun!

POSTED BY: CMRoberts , Lovington, NM
Overall rating: 5 out of 5 5 out of 5

I love this touch screen! I like to play FarmVille2 on Facebook, with the touch screen, I have much more fun than before!

My first laptop

POSTED BY: Tam , Jacobsburg, Ohio
Overall rating: 4 out of 5 4 out of 5

It's taking some getting used to, but so far I like my laptop. Really wish the battery would last longer. I'm still learning to use it as I had a desk top before.

Great computer

POSTED BY: kevmazz
Overall rating: 4 out of 5 4 out of 5

Great computer for the price haven't had any problems. The only thing I don't like about it is that you can not remove the battery. Mainly for the reason if your on a flight or in a meeting.. etc and your battery is about to die, you have to have it plugged in and cant have a back up handy. And the touch pad is in a weird spot feel like it can be moved a little to the right and is very hard to use. So I bought a wireless mouse and that works just fine.

Good laptop

POSTED BY: not applicable , na
Overall rating: 4 out of 5 4 out of 5

Have not learn all the feature of it. I don't like windows 8, Hard to understand. Need a tutorial on how to work it.

Solid Laptop, OK Touchpad

POSTED BY: Jack , NYC
Overall rating: 3 out of 5 3 out of 5

This machine works fine, but I dislike the touch pad, so much that I have bought a wireless mouse to use instead. The touch pad buttons are not well defined and it seems very sensitive-accidentally double clicks all the time. (I've tried adjusting the settings-no luck) The touch screen works very well though & the software is stable-no crashes.

something wrong here

POSTED BY: russ
Overall rating: 2 out of 5 2 out of 5

i bought a2.70 cpu laptop but the system said it is 1.80 i am confussed

Email bombardment

POSTED BY: DC momma
Overall rating: 2 out of 5 2 out of 5

I purchased a Toshiba laptop. This is the second one although I have purchased many more HP laptops and have been very satisfied with the laptops. Some of these were gifts for students. Toshibas bombardment of emails has annoyed beyond end. I will of course op out but this last survey request was it for me.

Worked Less Than 2 Weeks

POSTED BY: Just me , Long Island, NY
Overall rating: 1 out of 5 1 out of 5

This computer is the worst I've ever owned. It worked for less than 2 weeks before I started having all kinds of problems. The store that sold it to me didn't want anything to do with me. They told me that Toshiba doesn't make anything that's good.

MSRP: $799.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3337U Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L50 shop for accessories