Satellite L505-S5997

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Incredible Machine!

POSTED BY: Yoshi Matrix , Hayward, CA
Overall rating: 5 out of 5 5 out of 5

I just received this Laptop, and I must say it's incredible. I got this after using an IBM ThinkPad for a couple of years and while the IBM was a great laptop, this is all the better. Good Looking, great OS, quiet, fast, and multi-tasks like you would not believe. I highly recommend this laptop to everyone from the inexperienced to the professional user. For work or fun, This is the one.

the only things I would change about my toshiba

POSTED BY: Sandi , Atlanta, GA
Overall rating: 5 out of 5 5 out of 5

1 - the DVD door is right where I try to grab my computer if I am moving it. So far, I haven't ripped the door off but there is one edge that keeps clicking out of place and I have to push it back together. I suppose there is no perfect place but that is one I wouldn't have chosen. 2. The time between working on the computer and when it shuts down automatically is way way way too short. I wish it were just about 2-3 minutes longer but the manual discourages changing this due to some issue I can't remember at the moment. 3. For a music lover the speakers are just not quite loud enough for me. 4. could use a video tutorial on the mouse pad. I have had my machine since christmas and I'm still trying to figure it out.

Satellite is still the best

POSTED BY: Tessa , Honolulu, HI
Overall rating: 5 out of 5 5 out of 5

This is my third Satellite from Toshiba and I have to say it exceeded my expectations for a low cost lap top. My last on lasted 8 years and I expect to have this one for a long time. The funtions and features make it very efficiant to use.

MSRP: $679.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor T6600
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 memory
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories