Satellite L505-S5998

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

just dandy

POSTED BY: Rattlesnake , Westmnster, CA
Overall rating: 5 out of 5 5 out of 5

Received as a gift for Christmas from my wife. Our old laptop was getting pretty gritty. I think the Toshiba was a steal. The Windows 7 was a particularly nice surprise. Both our desctops are Vista. Win 7 cooks and required zip transition time. The intent was to use it (as we did our old one) almost exclusively for travel, but it is so much more powerful than our desktops and has more memory/storage that it's a shame to leae it in the suitcase. If only that bloody battery would hold up for more than an hour or two.

Very Good Laptop!

POSTED BY: trueladybug , Bakersfield, CA
Overall rating: 5 out of 5 5 out of 5

I have had no problems with this laptop. I use all programs without any trouble. It's built to least, very sturdy. The material is easy to wipe and least likely to scratch. Big keyboard is a plus when you are in college. The only thing, to my preference, is the laptop low volume. However, I have a jWIN amplifier with speakers, and it sounds fearless! Overall, this is a very good laptop.

POSTED BY: james , brownwood Tx
Overall rating: 4 out of 5 4 out of 5

This computer was is an all in one for what i do. the 10 key is a def add that i needed its speed is up there the things that i do not like about it is somethimes it will demagnify the screen, and the speakers are not that great but besides that its been pretty good so far

Short battery Life

POSTED BY: Tubutas , Fairyland
Overall rating: 4 out of 5 4 out of 5

Very good laptop, but even in eco-mode, has at most 1.5 hrs of battery-life.

Love my Toshiba Laptop

POSTED BY: Chestnuts , Erie, PA
Overall rating: 4 out of 5 4 out of 5

I have owned many computers in my life. The Toshiba Satellite laptop I purchased far exceeds the previous desktops and laptops I have owned. I spent alot of time and energy researching my next computer and the Toshiba brand kept popping up. I decided to purchase and I am not sorry that I did.

MSRP: $604.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor T4300
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 memory
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Realtek® 802.11b/g/n wireless LAN

shop for accessories