Satellite L505D-S5992

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent

POSTED BY: LDK , West Hills, CA
Overall rating: 5 out of 5 5 out of 5

Excellent product for the price.

Superior Laptop and Service

POSTED BY: Trish , Cheyenne, WY
Overall rating: 5 out of 5 5 out of 5

Buy a Toshiba and you will fall in love with the ease of use and the quality of the product and the service. You sincerely can't beat it for quality and price.

Best Laptop Out there

POSTED BY: Nina , Parkersburg,WV
Overall rating: 5 out of 5 5 out of 5

I love my Toshiba and have purchased our granddaughter one.

I love this laptop!

POSTED BY: none , Greensboro, NC
Overall rating: 5 out of 5 5 out of 5

When I told my daughter I wanted to get a laptop she recomended this one to me because she has owned one for over a year and is very happy with it. I was afraid it would be too hard for me to get the hang of but right from the start it was great. I would recomend it to anyone who wanted a great laptop for a great price.

Great Laptop

POSTED BY: Jo
Overall rating: 5 out of 5 5 out of 5

Received as a Christmas gift. Very pleased. Have purchase additional accessories: wi-printer, mouse.

Working Great

POSTED BY: Arrow , Boynton Beach, Fl
Overall rating: 5 out of 5 5 out of 5

This computer is performing very, very good. So far no problems and I do not expect any. The keyboard has the look and feels like a Desk top. The numeric keypad is an extra. The only thing I will add is another GB of memory (from 3 to 4). The 15.6 screen is nice and easy to read.

telling it like it is

POSTED BY: tall guy , Middletown, OH
Overall rating: 5 out of 5 5 out of 5

Toshiba overall has the best quality and the least amount of repairs when compare to other brands. I have another Toshiba labtop which is about 5 years old and never had a repair and I brought this new one for my wife. Researching, I found a study done by an insurance company for insuring against repairing computers and they showed that Toshiba was by far the least troublesome computer and in some cases were twice as better as compare to other brand names that had a greater maket share. I also talked with numerous other people including various sales clerks etc. and essentially they all agreed that Toshiba had better quality and less repairs than most other brands. On this particular computer, the AMD processor most definitely run hoter than anything else that I am accustom. Additionally, the AMD Vision recognotion is totally useless. It has never worked either for my wife or for myself. So if that is the reason for choosing this particular computer, I would advise against it. Otherwise the computer seems to be great.

PERFECT FOR 'NEWBIES'

POSTED BY: LORELET , Columbia, Md.
Overall rating: 5 out of 5 5 out of 5

Hi, this is my first 'lap' and I have to tell you that I did not have any problem at all, the guidance had help me a lot, the only sad thing is the battery's life (too short) but anyway, I love my 'new baby'. THANKS TOSHIBA

Perfect for all my Needs

POSTED BY: SM , Alexandria, VA
Overall rating: 5 out of 5 5 out of 5

I'm really enjoying all the features and most of all it was affordable....the only down fall is the battery life, but so far so good. Best investment for my buck. Glad I purchased it..

good all around laptop

POSTED BY: sammy , nc
Overall rating: 4 out of 5 4 out of 5

I have been using the computer for about 1 month and it is smooth and fast . Dont suggest to upgrade to 8g ram unless you have windows 64 bit It is heavy to carry on trips the battery life is only about 2.30 hrs and would prefer another hour of time aside from this a good computer.

Great Laptop

POSTED BY: Energy Convergence of NV , RenoTahoe
Overall rating: 4 out of 5 4 out of 5

This is a great laptop. I've had it for about 6 weeks and haven't had any problems. It's fast and the keyboard is great. If it had a longer battery life it would be perfect. Great business machine.

Good for the price

POSTED BY: Skydiver , Boynton Beach, Fl
Overall rating: 4 out of 5 4 out of 5

good quality product as expected from Toshiba. I'm just disappointed with the poor batter life and poor volume since I use my laptop primarily for sound.

Good

POSTED BY: Shuesplace
Overall rating: 4 out of 5 4 out of 5

Very good laptop, runs applications quickly and smoothly. Windows 7 looks and functions great on here. Battery life is alright, been getting about 2 1/2 hours of life. Its pretty light and doesnt get terribly hot with prolonged use. If your looking to play games on this i would recommend something else with a better graphics card. I bought mine refurbished, overall its a great laptop for the money.

needs more instructions

POSTED BY: Gene , Carlsbad, CA
Overall rating: 4 out of 5 4 out of 5

I like this computer , it runs smoothly without to much diffulty, however, it has a built in Voice and video , the video does and the voice part doesn't and I have been unable to find solution

New Laptop User

POSTED BY: PB
Overall rating: 4 out of 5 4 out of 5

What I like most about this laptop is the easy keyboard. It feels very comfortable typing on here. However they are leaving finger print marks of which I will need to know how to clean.

good basic computer

POSTED BY: wierdh52 , Smyrna, Ga
Overall rating: 4 out of 5 4 out of 5

I got the lap top to work with, and to play. I have enjoyed almost the whole experience. I would buy another.

Love My New Toshiba

POSTED BY: beaule207 , Litchfield, Maine
Overall rating: 4 out of 5 4 out of 5

I have always had a hard time typing on a lap top computer. With Toshiba the letters seem easyier to use to type with ease. I don't even mind e-mailing my friends now that I have my Toshiba. I found the price just right for me. It was less than half of what I payed for another brand and got all the same programs plus better ones at that!! Can't go wrong with Toshiba!

regular laptop

POSTED BY: jlona , los anglos ca
Overall rating: 3 out of 5 3 out of 5

hi i have a toshiba laptop which is satellite l505d-s5992, and i would like to ask you guys a question i have three bottom missing in my laptop. i realized that soon ago like 2 days ago. so i just want you guys to answer my question. Also i thank for those who made toshiba because is petty good and it's easy to use. Thank you for taking moment to read my review, have good luck and take care.

OK - POOR sound volume

POSTED BY: Muppet , Texas
Overall rating: 3 out of 5 3 out of 5

good laptop

POSTED BY: kperronne
Overall rating: 3 out of 5 3 out of 5

So far, this has been a great laptop for home personal use. This laptop was a gift for my wife to do her own personal surfing and avoid my work laptops and PC's. I cannot complain of any problems as of yet, it works great for her.

Sound needs improving

POSTED BY: sunny one , The Villages, FL
Overall rating: 3 out of 5 3 out of 5

I basically like this laptop and love Windows 7. However the speaker volume is much too low even when set to the highest levels. I think this a design fault and needs to be addressed by Toshiba soon. I have loved all my previous Toshibas but this one falls very short in the sound department. If this would be corrected, I would then be happy to recommend this computer to all my friends.

basic email surfing

POSTED BY: homer , qwest iraq
Overall rating: 3 out of 5 3 out of 5

I use this computer for emails, movies and surfing the internet. I have been very impressed with this computers performance. Only negative thoughts are the speakers are cheap, for the price I feel the speakers should be a little better and the battery is only good for one movie when traveling and there is no access to an electrical plug. Even when I use Eco mode I can only get one movie in. Do not recommend for traveling or listening to music but is good for at home use.

Webcam is tooooooo bad

POSTED BY: Notgood , Newyork
Overall rating: 2 out of 5 2 out of 5

I am disappointed with this laptop. The webcam resolution is horrible. I have tried all the possible options, but could not succeed in fixing the in built webcam.

MSRP: $599.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ II Dual-Core Mobile Processor M500
  • Windows 7 Home Premium (32-bit)
  • 3GB DDR2 memory
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Realtek 802.11b/g wireless-LAN

shop for accessories