Satellite L555D-S7005

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

best laptop ever

POSTED BY: ryan79 , Lima,Ohio
Overall rating: 5 out of 5 5 out of 5

i have had a lot of compters but i have to say the L555D-S7005 is the best i have ever had or used. the only down fall is the batter life.

Awsome lappy

POSTED BY: Evan , Franklin, IN
Overall rating: 5 out of 5 5 out of 5

I mainly bought this laptop to play online games(mainly Eve Online) and other media tasks and I must say I got more that what I originally thought I was getting. Combined with the Fusion application from AMD this by far is the smoothest laptop I have ever played on. I have had Dell, HP, Compaq and some others and I would definitely skip all them and get this one if I had to do it all over again. Very smooth laptop from the keypad layout to the .performance, 5 Stars Toshiba!

VERY SATISFIED:)

POSTED BY: NINA , PORT ARTHUR, TX
Overall rating: 5 out of 5 5 out of 5

THE OVERALL EXPIERENCE WITH THIS COMPUTER HAS BLOWED ME AWAY. I'VE HAD A TOSHIBA BEFORE AND I LOVED IT, BUT THE HARDDRIVE CRASHED. BUT THIS ONE WAS EXCELLENT AND HASNT HAD ANY PROBLEMS WHATSOEVER:) THE VERY BEST LAPTOP FOR SCHOOL, WORK, AND PERSONAL LIFE:)

great laptop

POSTED BY: travise , ept
Overall rating: 5 out of 5 5 out of 5

recommend this laptop, great value, great screen, windows 7 is awsome!! fast performance.only down side is the keyboard(noisy). other than that A+++

little white lie?

POSTED BY: RUSS
Overall rating: 4 out of 5 4 out of 5

Nice computer. Only problem i had is that it says on the sticker that is has 64bit windows7 installed but has 32bit instead. Battery life is real short. And bluetooth would have been nice.

Satisfied but...

POSTED BY: Robert , Lubbock, TX
Overall rating: 4 out of 5 4 out of 5

I like the machine alot but one glaring problem is that I get the dreaded blue screen. There does not seem to be any consistent pattern. Updating my iphone, watching a movie, writing in Word or working in Excel. Checking on internet for some solution, others mention the problem but Toshiba isn't offering any solution or doesn't seem to be acknowledging the problem. Makes me a little wary when using it. Go figure.

good laptop

POSTED BY: liz , tampa, fl
Overall rating: 4 out of 5 4 out of 5

im in college and i have to take computers and technology class and my professor was impressed with my laptop so that might just say it all.. and i love it too

disapointed

POSTED BY: mack-1 , springhill FL
Overall rating: 3 out of 5 3 out of 5

speed is satisfactory startup and shutdown, no hdmi no lableflash and a weak realtek wireless card

MSRP: $649.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ II Dual-Core Mobile Processor M520
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR2 800MHz memory
  • ATI® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive

shop for accessories