Satellite L645-S4059 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Exceptional value

POSTED BY: psychlotron , Austin TX USA
Overall rating: 5 out of 5 5 out of 5

This unit is a near-ideal balance between price and performance. Keyboard is nice, seems like the spacebar is a little touchy but no major issues. Speakers aren't great, but small speakers never are. "Real world" battery life is more like 3-4 hours depending on application. I consider those issues minor, and they are far outweighed by the performance of an i3 with 4GB DDR3 SRDAM. 14" display is very good looking and not as clunky as 15.6" or larger. I caught this laptop on sale for $549.00 and call that a bargain, the best I've ever had.

My second Toshiba Laptop

POSTED BY: AsoG , Pharr, TX
Overall rating: 4 out of 5 4 out of 5

my only problem with this laptop is the fonts are too small for old eyes but the magnifying tool is helpful, but takes some getting use to.

Good Budget Business Laptop

POSTED BY: paulg , Southeast
Overall rating: 4 out of 5 4 out of 5

Good budget business laptop.

poor battery life

POSTED BY: hawkeye79 , Appleton, WI
Overall rating: 3 out of 5 3 out of 5

I have charged and discharged the battery several times to "condition" it. One reason I chose this particular laptop was the listed battery life. I don't expect it to actually match what is listed, but when one does not even get half that, I am disappointed. If the battery life was a bit better, this would be a good laptop for the price.

concerned

POSTED BY: sofbaldad , Visalia, ca
Overall rating: 3 out of 5 3 out of 5

The computer is not operable at the moment. Runs super slow. takes minutes for screens to refresh.

MSRP: $674.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-370M Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories