Satellite L655-S5105 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Cannot go wrong with Toshiba

POSTED BY: jnbarx , Mentor, OH
Overall rating: 5 out of 5 5 out of 5

Needed to replace desktop with laptop and took the time to research many brands to meet my business needs. Toshiba came out way ahead. Nothing to complain about except speakers. Sound not the loudest, but not important to me. Highly recommend this model and if you can find them at MicroCenter, get them now, going fast!

Overall rating: 5 out of 5 5 out of 5

Lightning quick speed. In comparison to my girlfriends Apple Macbook the load time on my L655 is a few seconds quicker! The only nag is the battery life. The first few days we're great but its gotten a bit worse. Overall I'm very satisfied with the purchase and would recommend it to anyone looking for an affordable, quick and stylish laptop.

Pretty Good

POSTED BY: Someone , New Jersey
Overall rating: 5 out of 5 5 out of 5

I bought this laptop new so far its pretty good but im kind of suspicious of the battery after reading the comments and seeing the rates for it for the battery but i hope it wont turn out bad so far i recomend this laptop...

So Far, So Good

POSTED BY: Geek , Philadelphia, PA
Overall rating: 5 out of 5 5 out of 5

We just picked up this computer two days ago and so far, we are very pleased with our purchase. The computer is very fast and appears to be of high quality. Most of the software we needed was pre-installed. Even Google Chrome was set to go. The only thing we had to do was buy some DVD's to create Recovery/Restore disks. These are no longer standard with new computers, so you have to roll your own. Oh, we had to uninstall Norton Anti-Virus as we use Microsoft's product. You only get about 281 GB of usable space out of the 320 GB hard drive. I think there are hidden files out there. Of the 281 GB, 21 GB was used by pre-installed software including windows 7. So that leaves you about 260 GB for your files. More than we need, but might be tight for some people. But I guess you could always delete the hidden files to get you more space. Overall, we are very pleased.

Very Reliable Laptop

POSTED BY: PG , Copiague, NY
Overall rating: 5 out of 5 5 out of 5

This laptop has all the features that I need & it is easy to use, It's not too heavy so it's easy to transport.

Cool Laptop

POSTED BY: hand851 , Columbus, Ohio
Overall rating: 5 out of 5 5 out of 5

This laptop is awsome.

Superb Laptop Comuputer

POSTED BY: R , San Jose, CA
Overall rating: 5 out of 5 5 out of 5

This computer is really wonderful, the screen is crystal clear, the keyboard is flawless and the speed and quickness is outstanding. Ultra sleek, quiet as a mouse. This i3 processor is far superior than my HP and Dell that i had previously. Everywhere I take my laptop I get complements. I am very pleased with my purchase.

Great Value

POSTED BY: Mark , Cleveland, OH
Overall rating: 4 out of 5 4 out of 5

A "everything" you need laptop, without the big price tag. My wife and I have been very pleased.

Great Computer!!!

POSTED BY: Chuck , Boston, Mass
Overall rating: 4 out of 5 4 out of 5

Easy to set up, went right to work. Speakers are not the best quality, but adequate. Love all the new features, compared to my old desktop clunker.


POSTED BY: cobollover , Garden City, NY
Overall rating: 3 out of 5 3 out of 5

Nice laptop, a little wider than my Dell Inspiron. No bluetooth. WIFI keeps dropping even when I am within 10 feet of my router. Toshiba has no answer.

Speakers are pitiful

POSTED BY: snell613 , Houston, TX
Overall rating: 2 out of 5 2 out of 5

I bought this laptop to replace a 6 year old Satellite, assuming that I would get the same outstanding sound quality. Instead, the speakers sound tinny and have very little volume. Also, although I am not a fan of full-sized keyboards, the layout of this one is particularly bad. If I could avoid a re-stocking charge, I would exchange this laptop for a Dell 15R, which has similar specs. For $50 more, the Dell provides a larger hard drive, bluetooth, and much better sound quality.

MSRP: $669.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-370M Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories