Satellite L655-S5117 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

The best computer for that price

POSTED BY: Mike
Overall rating: 5 out of 5 5 out of 5

I bought this laptop 1 month ago and I love it! It has a really good performance and is really fast. I enjoy using it to watch movies because of its high quality images. I work a lot with numbers and Excel for that reason the number pad is really useful.

Fast and Sleek, hot rod style

POSTED BY: medic1950 , walterboro,South carolina
Overall rating: 5 out of 5 5 out of 5

This is my fourth Toshiba and I have been owner of HP and Acer. This by far is the best deal I have ever found. 64bit 4G ram 320GB hdd. Light with long battery life. I have not had any Problems with any Toshiba laptops yet. This one is fast and easy to setup. love homegroup and other software. I own a Toshiba A505-6960 6980 6025 and now the l655-s5117 I highly recommend Toshiba to everyone.

easy to use

POSTED BY: lucky , Ocala fl.
Overall rating: 5 out of 5 5 out of 5

easy to learn, many more features than my other computer, kighter wieght. and a great keyboard. love love love

POSTED BY: wooty
Overall rating: 5 out of 5 5 out of 5

Affordable. Great value.

great for the price

POSTED BY: mammazano
Overall rating: 5 out of 5 5 out of 5

Got it at a great price for all that is included. Has more than I need most of the time but is great for future plans I have for both work and home use.

First laptop

POSTED BY: Mick , Bakersfield, CA
Overall rating: 5 out of 5 5 out of 5

After having PC's for years and seen and used older laptops I was convinced I would never want one. Then my son brought his new Satellite by. Its better than my latest PC with larger keys making it easier to use as well as faster. Great machine

Amazing Laptop

POSTED BY: Blue Eyes , Lebanon,NH
Overall rating: 5 out of 5 5 out of 5

Amazing laptop, amazing price! I have already recommended to my friends.

Great Computer!

POSTED BY: DB
Overall rating: 5 out of 5 5 out of 5

This is a great computer. This is our second Toshiba and so far we are huge fans! My ONLY complaint is that the USB slots are at the front right hand corner of the computer. So plugging in a wireless mouse you are always bumping into the USB part of the mouse. I did get a nano mouse which helped but I would have preferred them to the back of the computer or on the left side. No huge deal thought. GREAT computer and very, very happy with the purchase.

POSTED BY: Bo , Pa
Overall rating: 5 out of 5 5 out of 5

I am very pleased with my new purchase

Awesome!

POSTED BY: jase , lake elsinore
Overall rating: 5 out of 5 5 out of 5

This is definently, a leap from dell. So much better and love the updates for everything. Customer support is ridiculously great and cant explain how much more i love these computers!

Stepping Up

POSTED BY: Obzealous , Erie, PA
Overall rating: 5 out of 5 5 out of 5

I love my new laptop! When using it (which is often) I feel like I'm flying. It's responsive! It gets me where I want to go quickly and I look forward to a long and happy relationship.

First laptop ever!

POSTED BY: skippy , Milwaukee
Overall rating: 5 out of 5 5 out of 5

I'm very pleased with my purchase!

POSTED BY: Bob , Sudbury, Massachusetts
Overall rating: 5 out of 5 5 out of 5

would like to have hdmi port. I don't care for the finish because it shows hand prints. I don't use the battery, removed after initial charge and put aside. battery has easy acess.

Good notebook for a very good price.

POSTED BY: Rincewind , Malvern, PA
Overall rating: 5 out of 5 5 out of 5

Everything seems to be working great. The only complaint I've got (and it's a bit nit-picky) is that it could you one or two more USB ports. It's kind of a pain having to swap things around constantly when it only has two.

Incredible deal, great computer

POSTED BY: medic1950 , walterboro,SC
Overall rating: 5 out of 5 5 out of 5

Beautiful screen, fast and loaded with great features. 64bit 4gb ram. lasted almost 6 hours on a charge. This is my 4th toshiba and have never had any problems with any of them. This is very light and a pleasure to use. You just gotta be lucky enough to find one now. good luck

Best price on best laptop.

POSTED BY: urangg , Las Vegas, NV
Overall rating: 5 out of 5 5 out of 5

At first i thought is was a mistake. A core 3 processor at that price was too good to be true. But it wasn't a mistake and i jumped on it.

AWESOME

POSTED BY: Steve , Crofton, MD
Overall rating: 5 out of 5 5 out of 5

Absolutely love this laptop...big screen...great keyboard...easy to set-up.....

Great Laptop

POSTED BY: LGH , Tampa, FL
Overall rating: 5 out of 5 5 out of 5

Good laptop, efficient, fast, great for the $$.

great

POSTED BY: boney
Overall rating: 5 out of 5 5 out of 5

easy to use

Addicted to TOSHIBA

POSTED BY: needmoney
Overall rating: 5 out of 5 5 out of 5

This is my second TOSHIBA Laptop, and I'm extremely happy with it. The first one was a true "veteran" that served more than four years, before I decided that is time for new recruit! Personally, for me, this model was the best choice not because I'm addicted to TOSHIBA but rather that it was the BEST choice for the price, processor and memory. I read in previous comments that some users were complaining from the glance coverage and the numerous fingerprints, other were complaining that the touch pad is slightly to the left of the laptop, BUT is perfectly centered to the keyboard. I don't any problems with these issues. Since the first TOSHIBA that I still have I highly recommend this brand of laptops to anyone that I know. I even convinced some of my most prejudice friends to buy Toshiba instead of Sony... So far, no one is complaining of their choice. If you are looking for a highly reliable laptop for everyday use this the right choice!

Great performance, great price

POSTED BY: Billi , miramar, FL
Overall rating: 5 out of 5 5 out of 5

This is a very good laptop. I'm very satisfied with the purchase !!!

Great Laptop

POSTED BY: Rozelle , Beltsville, MD
Overall rating: 5 out of 5 5 out of 5

Core i3 processor sets this laptop apart. Great full-sized keyboard and large LCD display make it very easy to use. Has all the essential features I need for business and pleasure.

new laptop user

POSTED BY: Dee , Menifee, CA
Overall rating: 5 out of 5 5 out of 5

I have used a desk pc for a long time, but this is the first laptop for me. My friend helped me pick it out and it is the best one that I saw. I am very happy with it.

Great Laptop for Great Price

POSTED BY: RightOne , Evansville, IN
Overall rating: 5 out of 5 5 out of 5

Satisfy tweens AND adults with this great product.

SATISFIED

POSTED BY: pappy , coraopolis, pa.
Overall rating: 5 out of 5 5 out of 5

NOTHING TO COMPLAIN ABOUT, COMPLETELY HAPPY

Excellent laptop for the price

POSTED BY: Aflac man , Franklin, VA
Overall rating: 5 out of 5 5 out of 5

I really enjoy this laptop. I like the built in numeric pad. The unit is fast and light weight, while providing lots of power and speed.

Great Laptop for the price

POSTED BY: Hot South
Overall rating: 5 out of 5 5 out of 5

It's just as far and powerful than more expensive models

Best Birthday Present

POSTED BY: CAHappy , San Diego, CA
Overall rating: 5 out of 5 5 out of 5

Rec'd as a birthday present & couldn't be happier

Satelite L655 series

POSTED BY: Jody , Cleveland,Ohio
Overall rating: 5 out of 5 5 out of 5

I am truly enjoying my new laptop. it is one of the best investments i have made over the last 2yrs. I have refered several class mates 2 pruchase the exact brand and model. I truly hope i do not exsperience any technical difficulties, thank u toshiba.

excellent value

POSTED BY: jt , concord, nc
Overall rating: 5 out of 5 5 out of 5

Will do more than I would ever need

POSTED BY: BL
Overall rating: 4 out of 5 4 out of 5

Does not have HDMI slot, otherwise exceptional price.

Value, low maintenance laptop!

POSTED BY: Moonbeam , Murray, KY
Overall rating: 4 out of 5 4 out of 5

Good replacement for my 2005 Dell! Has all the features I need, mainly for home use and internet browsing.

Good value for the price!

POSTED BY: Tech Junkie , IN
Overall rating: 4 out of 5 4 out of 5

Good laptop, plenty of speed, Windows 7 runs quick. Sufficient hard drive space, ram, and processor for the price. Looks good, battery life is good. Only issue is the viewing angle of the screen. You almost have to tilt the screen back a little bit. Looks great though, for the price i love it!!!

Great value

POSTED BY: smhood , Hartford, CT
Overall rating: 4 out of 5 4 out of 5

I was looking for a value laptop that offered the latest software and hardware, decent memory size, and good battery life but at a reasonable price. All in all a great laptop that has quick performance and some neat features for a medium-user like myself.

one of a kind!

POSTED BY: dani , brownsville,TX
Overall rating: 4 out of 5 4 out of 5

one of a kind in advanced computers

Good, reliable machine

POSTED BY: Nursedawg , Newport News, VA
Overall rating: 4 out of 5 4 out of 5

I was looking for an inexpensive simple reliable laptop. It was relatively inexpensive and I expected the worst. I was pleasantly surprised. It handles multitasking well and the full sized keyboard is a plus. It is also possible to get 4+ hours of use out of the battery. The camera image is sharp and great for Skype.

adequate

POSTED BY: vonnie , bloomfield, nj
Overall rating: 4 out of 5 4 out of 5

this model is adequate. there are no special features, the battery life is mediocre, and it is heavy. however, it performs well and is reasonably priced. no major complaints, but nothing to write home about either.

Great value, touchpad needs improvement

POSTED BY: Mike , Hillsborough, NC
Overall rating: 4 out of 5 4 out of 5

The performance of this laptop is great and I love the extra storage. The touch pad location takes some getting used to - it's off-center due to addition of numeric keypad. Too early to speak on battery life. Quality of display is a little grainy/blurry given today's technology. Would give the unit a solid B.

Best Laptop for daily use

POSTED BY: Praveen , Providence, RI
Overall rating: 4 out of 5 4 out of 5

First, let me tell you that Toshiba Satellite L655 is great value for money . It has the features which I required (except top end graphics, however, I am not interested in playing games, that said). I miss Gigabit Ethernet; since this laptop only supports 10/100 Ethernet interface, so if you thinking of transferring files between systems will be slower. Second, does not have HDMI port. And no anti-glare coat on the screen, will be difficult to use in sun light. I have already recommended this laptop to my friends, however, it was out of stock within hours, I hope they stock enough for customers. Best of luck

Laptop Review

POSTED BY: ibewise , Clarkston, MI
Overall rating: 4 out of 5 4 out of 5

I like the Toshiba. For the price, it has a lot of nice features.

bad speakers

POSTED BY: bill
Overall rating: 4 out of 5 4 out of 5

I like the computer a lot. but the speakers do decrease the joy of using the computer.

Good laptop

POSTED BY: blonette
Overall rating: 4 out of 5 4 out of 5

This is a really good laptop. I have been very satisfied with the speed and performance of this product. I would like it better if it had a little bit longer battery life, but over all I am very satisfied.

Pretty good

POSTED BY: Geek Squad is cool , New York, NY
Overall rating: 4 out of 5 4 out of 5

I am a light computer user. I use my laptop for surfing, uploading pics and storing them. I am still learning the features of my new computer, but have a complaint. I do not like the touchpad. When i move my finger around on it, somehow it increases or decreases the size of the screen. It is quite annoying especially since i do not know how to fix it once it happens. I also dont love the buttons under the touchpad-i dont find them as comfortable as my work laptop. But to be fair the computer is quick, smooth and sleek.

a good one

POSTED BY: doc , bronx
Overall rating: 4 out of 5 4 out of 5

good laptop as battery lifes more than 3 hrs,all suficient features with core i3 processor at such economic price..

I'm happy with it.

POSTED BY: tommygun , Cincinnati
Overall rating: 4 out of 5 4 out of 5

A friend who does laptop repair at a major office supply store recommended Toshiba over all other brands. He claims that Toshiba laptops are the most reliable. That was good enough for me. Mine has performed flawlessly since day one.

POSTED BY: jj , Southington, CT
Overall rating: 4 out of 5 4 out of 5

Solid basic notebook.

Very nice laptop, esp for the price

POSTED BY: Steph , Logan, UT
Overall rating: 4 out of 5 4 out of 5

Very nice laptop, and an excellent deal for the price! It works very fast, looks nice, and has a great screen for watching movies, TV shoes, etc. Speakers aren't even that bad.

Non locking lid

POSTED BY: Lou , NY
Overall rating: 3 out of 5 3 out of 5

Lid closes like a book. It does not latch. There is nothing to keep the lid from opening when carried.

Not very Pleased

POSTED BY: Ann , louisiana
Overall rating: 3 out of 5 3 out of 5

Laptop seems to run slow especially since I have very little downloaded on it. I chose Toshiba over your competitor as I previously owned one. Thought sure a 4GB was going to be a charm. Isn't the case! What a shame!

First laptop

POSTED BY: Mom , Central, IL.
Overall rating: 3 out of 5 3 out of 5

For my first laptop I really like it. Use the net a lot more.Able to do things with laptop I couldn't do with my old computer. Have to play with it more.

Good Value

POSTED BY: Bill , Niceville, FL
Overall rating: 3 out of 5 3 out of 5

The L655 Laptop has functioned well overall and the Battery life has been better than expected. However, during the first month I have used it, Windows has shut down for unknown reasons several times. It has rebooted successfully so far and has not shut down in the last 4 days.

No paper documentation

POSTED BY: Jumping Jack
Overall rating: 3 out of 5 3 out of 5

I realize that the manual may be found on-line, but it would have been nice to have at least a starter booklet to refer to.

First laptop

POSTED BY: suziQ , Englewood, FL
Overall rating: 3 out of 5 3 out of 5

Does everything you need; has convenient card reader and USB ports. Not a lot of junk preloaded on it but some. Shiny finish shows finger prints; a textured finish would be more practical. Battery life has been very poor. Lucky to get 2 hours; literature says it should get over 5. Overall, for the money, a good buy.

Dissappointed - Not as expected

POSTED BY: ED , St Petersburg, FL
Overall rating: 2 out of 5 2 out of 5

The speakers/sound is really poor. It is too heavy to take around with you. I wish I could trade it in for a different model. Don't buy a Laptop with a camera - You can't move it unless you move the screen ! Buy an aftermarket camera.

Very sensitive to minor movement

POSTED BY: Colleen , Raleigh, NC
Overall rating: 2 out of 5 2 out of 5

I find that I must spend a considerable amount of time correcting errors that come about from very minor movements while working on the computer

Returned

POSTED BY: d , Bedford, TX
Overall rating: 1 out of 5 1 out of 5

I purchased this computer and 3 days later it crashed. I exchanged it for the sme computer and it crashed the next day. I reutrned that computer and purchased a different brand that I have not had any trouble with at all. I will never purchse a Toshiba again.

Difficult to use this computer

POSTED BY: Richie , Mid-Michigan
Overall rating: 1 out of 5 1 out of 5

I am not happy with this laptop. It is not very ergonomic. The keyboard is hard to use. The depressions on the keys are so slight that it is difficult to tell if you ore "on" a key or not. The littl bumps on the "F" and "J" keys are too small to feel, so you have to look to see it your fingers are on the right keys or not. The keys have almost no space between them so it is very easy to "fat finger" this keyboard and get two keys at a time instead of just the one you are trying to get. Then there is the touchpad -- it is also very frustrating and difficult to use. There is no edge on the touchpad to let you feel where you are -- the touchpad the same level as the panel in which it sits so you can not feel where you are. The touchpad is also almost the same color as the panel, so you can not tell where the touchpad is by looking unless you have very good lighting. I am sorry that I bought this laptop. On top of all the ergonomic problems, this laptop is also a fingerprint and smudge magnet-- it is impossible to keep it clean because of the super shiny finish on the case.

MSRP: $620.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-370M Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories