Satellite L675-S7112 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»


POSTED BY: The awsome , raleigh, nc
Overall rating: 5 out of 5 5 out of 5

The bugs are the keyboard. my 6 key came off but was repairable, and it just feels weird. Another bug is the mouse area, where you click. Little stuff like crumbs, etc can get stuck and stop left click from working. I guess when it was too late toshiba realized that that would happen, so they made it where you move the arrow you double tap it you click. Other than that stuff, this laptop ROCKS!

Best Laptop to own!

POSTED BY: scots331972 , Calumet, MI
Overall rating: 5 out of 5 5 out of 5

I have had my laptop for 1 year now and I have never had any problems with it. I use it for games and school and it does the job it was purchased for. I would recommend any Toshiba laptop to anyone out there looking for the best computer for any need.

Good overall

POSTED BY: bugz , silver city nm
Overall rating: 3 out of 5 3 out of 5

This is a good laptop. The only thing it should have is a backlighted key pad.

Keypad problems

POSTED BY: TATAN , Puerto Rico
Overall rating: 2 out of 5 2 out of 5

I'm having problems with the keypad,the mouse pointer keeps jumping and i can't control it unless i use an external mouse.

Very bad laptop

Overall rating: 1 out of 5 1 out of 5

HDD die

MSRP: $759.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-380M Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • Blu-ray Disc™ ROM (BD-ROM) and DVD SuperMulti drive with Labelflash®

shop for accessories