Toshiba Satellite L75-A7380 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Fantastic Laptop

POSTED BY: Wendlebaby , Wheelersburg, OH
Overall rating: 5 out of 5 5 out of 5

I am not a very savvy tech person but I have found using the Toshiba Satellite Laptop to be very easy and convenient. I would recommend it to others.

Toshiba laptop is great

POSTED BY: WI laptop user , Rhinelander, WI
Overall rating: 5 out of 5 5 out of 5

I am learning to appreciate the luxury of sitting in my living room while working on my laptop. I like the 17" screen size and the keyboard layout. The best thing about this laptop is its speed! I do wish the battery life was longer though.

Excellent, so far!

POSTED BY: mommy , Far Rockaway, NY
Overall rating: 5 out of 5 5 out of 5

I got this laptop as a gift from my daughter, when my old laptop died. Its taking a lot getting used to because of the change from windows 7 to windows 8. Overall,the speed is good and the words and display is very clear. The laptop does not overheat like my last one. I'm still learning about the features, and having fun. My husband uses the Toshiba laptop for his work and seems very satisfied.

Toshiba Satellite L75-A

POSTED BY: mac
Overall rating: 4 out of 5 4 out of 5

Good Laptop but Microsoft Windows 8 is a disaster. New Metro and Apps not designed for Personal use. Feel bad for Corporate Companies using this version.

windows 8 is a sad joke

POSTED BY: jayway , vt
Overall rating: 3 out of 5 3 out of 5

Look, this is a decent laptop for the money. The main problem is the Windows 8 OS, it is a ridiculous piece of garbage. I don't want my computer to be my phone, I don't want apps, I want programs. If you can deal with windows 8 then have at it.

Dissappointment

POSTED BY: Hotes , Albany, NY
Overall rating: 3 out of 5 3 out of 5

I have owned Toshiba laptops in the past and have been quite impressed with them, but this time was a total failure. First off, Windows 8 is a failure in itself and when I tried to upgrade to 8.1, the system would not do it. It tried to, but failed on each attempt. The touchpad also had issues. At first I thought I was doing something wrong, but in retrospect, there must have been something wrong with it (mind you this was a brand new machine), because it did not operate correctly.

POSTED BY: First Time Toshiba user
Overall rating: 2 out of 5 2 out of 5

I was expecting the PC more than I am receiving. However, this i5 computer performs slower than my i3 cheaper computer. The keyboard is a big disappointment. Consistently missing key is the problem. I wish I did not purchase this computer because missing keys is very irritating.

MSRP: $623.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3230M Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L70 shop for accessories