Toshiba Satellite L75D-A7288 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best Laptop Ever

POSTED BY: Miranda , GA
Overall rating: 5 out of 5 5 out of 5

I replaced my Acer laptop with a Toshiba laptop. I had loved my Acer, but my new Toshiba is even better! With a Toshiba Satellite L75D-A7288 Laptop, you won't be disappointed.

Good value

POSTED BY: Southbound27 , Greensboro, NC
Overall rating: 5 out of 5 5 out of 5

The cpu is up-to-date and powerful. I picked it because of the removable chip feature that Intel does not have.

great laptop

POSTED BY: CAROL , NEWNAN, GA
Overall rating: 5 out of 5 5 out of 5

this is my second Toshiba and I think they are great laptops.

Love It

POSTED BY: CJ , NC
Overall rating: 5 out of 5 5 out of 5

It is a very fast laptop. the only thing that bothers me is that the mousepad is not centered - its off to the left of center. I love the large, clear screen

Programmer/Photograher/Photo Editor knows Tech

POSTED BY: DeFive Studios , Maryland
Overall rating: 5 out of 5 5 out of 5

The L75D-A7288 is an excellent, beautiful machine, I normally build and program computers for friends and family but I needed something Now not Later, I couldn't wait so I purchased this model on the fly with low expectations because simply it wasn't built by me so I didn't know what was exactly in it, I mean I read the box but that doesn't say much, anyway this machine has surpassed every expectation I have had, I have been able to edit photos in photoshop and lightroom faster than the last computer I had bought which was an Acer. which over time I upgraded myself. This machine hasn't needed any upgrades it runs smooth, and I'm happy with the battery life, for a 17'" screen the battery is more than capable, people complaining about battery life need to realize bigger computers demand more power, and you can always find after market batteries that last longer if that's your problem. Overall this Computer is more than capable for running anything you can possibly throw at it, and if need be you can always upgrade the internal memory, video cards and ram. I love it.

MY LAST COMPUTER WAS A TOSHIBA

POSTED BY: 4X4 , CT
Overall rating: 5 out of 5 5 out of 5

LOTS OF SPACE AND SNAPPY FAST. I LIKE IT.

POSTED BY: Phil , Imperial,Mo.
Overall rating: 5 out of 5 5 out of 5

This is my 3rd Toshiba, think they are top of the line

cannot change the mouse pad

POSTED BY: woody , port charlotte, fl
Overall rating: 3 out of 5 3 out of 5

The mouse is very hard to hit. I changed the sensitvity but it didn't help. Is there a light on the keyboard?

average laptop

POSTED BY: flyguy , TN
Overall rating: 3 out of 5 3 out of 5

With the size of memory and HHD installed I would have expected better performance. Battery life is poor. Comes with Norton Anti-Virus which is a poor program. I got a virus on computer in less than a week of owning this. Had to restore to earlier point.

MSRP: $599.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A8-5550M Accelerated Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • AMD® Integrated Graphics
  • 1.0TB (5400 RPM, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

build your own L70 shop for accessories