Satellite L745D-S4230 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Satellite L745D-S4230

POSTED BY: ShreadEagle , San Antonio, Tx
Overall rating: 5 out of 5 5 out of 5

Awesome Laptop! Speed, Perfomance, and Battery Life are excellent!

great machine just what I needed

POSTED BY: LARRY , lubbock, tx
Overall rating: 5 out of 5 5 out of 5

Does everything I needed a great 14 inch laptop. I needed one to power up quick and do what I needed to do in a fast moment.

Satellite L745D-S4230 Laptop

POSTED BY: Geezer
Overall rating: 5 out of 5 5 out of 5

This laptop is by far my favorite. Beautiful style and clear screen. Everything about this laptop makes it the best I ever had (so far). I did how ever notice 4 minor flaws that might just be the way I use my laptop. The SPACE BAR and the LEFT CLICK button next to the Touch Pad needs to be pushed a little harder in order to work. Next is the AC Adapter cord. The plug that goes into the side of the laptop sticks out too far. In the past, I have seen this type of connection fail do to pressure on the plug causing to damage the internal connection. The last item is the speakers, older models had louder speakers.

Good all-around laptop

POSTED BY: Serjoza , Novi Sad, Serbia
Overall rating: 5 out of 5 5 out of 5

Have it for a month now. Fast, light weight and also beautiful design. Great monitor in the sense of colors and brightness but with low angle of viewing. Also, stays cool even after hours of extensive use. As for cons - too many unnecessary light indicators, space button is slightly less responsive than it should be, and the speakers are better on my cellphone than on this laptop. All in all, great all-around and reliable machine for the money you pay.

Good laptop for function and speed

POSTED BY: eagle
Overall rating: 4 out of 5 4 out of 5

I've had this laptop for about a month now and have not had any issue with it. It boots up quickly and is almost too fast for me, but I'm getting used to it. The battery life is not as good as stated and non-Toshiba extended batteries don't work, so looking at getting a Toshiba extended battery. If you don't need to have more than 3 hours battery life, this one will server you well. I would recommend it.

MSRP: $599.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A6-3420M Accelerated Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories