Satellite L755-S5246 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Good computer

POSTED BY: HankHill , Nashville
Overall rating: 5 out of 5 5 out of 5

Volume control is not easy to use.

these are the best

POSTED BY: frankied , Hampton, Va
Overall rating: 5 out of 5 5 out of 5

This the second toshiba laptop that I purchased and in my opinion they are the best. I really appreciate the full number pad. They also come in colors that are not an additional cost. Battery time is the biggest draw back. However, these are Super values!

Great Student Computer

POSTED BY: StudentS , Omaha, NE
Overall rating: 5 out of 5 5 out of 5

I purchased this computer for use as a college student. It has been such a great tool so far! The battery life is wonderful, the speed at which it runs is fantastic, the features are excellent and the overall look of the computer is so sharp-I get so many compliments on it! This was a great computer to purchase at such a low price!

Wonderful laptop

POSTED BY: Sam , Rochester Hills, Mi.
Overall rating: 5 out of 5 5 out of 5

This is my third Toshiba laptop computer purchase. Each one has performed wonderfully, with none having to be returned for service. The features are all easy to use, the screen is easy to view, and the battery remains usable for long enough to complete my work without recharging.

Best Bang for the Buck!

POSTED BY: Handler , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

A great value - super fast performance, a ton of memory, and excellent power management to extend battery life

Very Nice

POSTED BY: Alfred Hitchcock , Sulphur,LA
Overall rating: 5 out of 5 5 out of 5

Toshiba makes a quality laptop that performs well and looks nice. I am very satisfied with the computer. The screen is clear and crisp. Everything functions as I had hoped it would.

SO PLEASED

POSTED BY: SHE , Willis,TX
Overall rating: 5 out of 5 5 out of 5

Light in weight. Easy for a newbie to use. Has all the most desirable features.

Wonderful laptop

POSTED BY: ChinaDave77 , Florida
Overall rating: 5 out of 5 5 out of 5

I am still learning the benefits and advantages of this laptop. I am very satisfied.

Great performance

POSTED BY: mrjimmer , USA
Overall rating: 5 out of 5 5 out of 5

I read a lot of reviews about this Toshiba, some good, some bad. So when I got my Satellite I was a little skeptical, but I have to tell you that this laptop tops my other laptop (HP pavilion dv4) by miles, ie; larger keys, three USB outlets, faster, easy to use and understand, great price. Overall a really good computer..

very good laptop....amazing!

POSTED BY: schwarz , tamilnadu,india
Overall rating: 5 out of 5 5 out of 5

woww....i just love it...first i was thinking that it's processor was not good ...but later on i came to know that its better than the i3!!!

Excellent Product

POSTED BY: Dr. D , Baltimore, Maryland
Overall rating: 5 out of 5 5 out of 5

I am extremely pleased wtih the computer. It works easily and I can usually do more than I even intended to do. The work looks great when printed out.

First Laptop

POSTED BY: Chuck , Portland, OR
Overall rating: 5 out of 5 5 out of 5

Improve programs that come nalready loaded, i.e. expand Microsoft Word.

I can actually USE it!

POSTED BY: Fred , Berkley, MI
Overall rating: 5 out of 5 5 out of 5

I love the way it looks, feels when I type on the key board. I am impressed that I have figured out so many of the features. I bought this because my son who is a tekkie in Seattle, picked it out for me saying, my previous computer was a "dinosaur." I have not yet used my new laptop outside the house or even unplugged it.

My 3rd Awsome Toshiba Laptop

POSTED BY: Chuck , Washington, DC
Overall rating: 5 out of 5 5 out of 5

Toshiba consistanly delivers high quality. This is my 3rd Laptop and I still use my original one I purchased nearly 10 years ago. It is super light and runs very cool. It is fast and very well made. My only request is that Toshiba would make a bootable DOS disk utility for Toshiba Brand Hard Drives.

Excellent Laptop for everybody

POSTED BY: chake , La Romana, R.D.
Overall rating: 5 out of 5 5 out of 5

I love my computer. It is wonderful and so cut for me and for you too.

Great Buy!

POSTED BY: sunlover , Pittsburgh, PA
Overall rating: 5 out of 5 5 out of 5

I'm in my sixties and wanted to get a new computer. This one seemed to fit my needs and budget!

Nice Laptop

POSTED BY: User35 , Missouri
Overall rating: 5 out of 5 5 out of 5

Seems to be a very good laptop. 100% better than the previous one I had which was NOT a Toshiba. Does everything I need it to do.

laptop experience

POSTED BY: geraldo , Kennewick, WA
Overall rating: 5 out of 5 5 out of 5

I owned a laptop 10 years ago and than went to a desktop and now to this toshiba laptop and so far I am very satistified

Great!

POSTED BY: TheBryan , Nashville, TN
Overall rating: 5 out of 5 5 out of 5

Fast and reliable!

Great laptop!!

POSTED BY: cookboi , Fort Waye, Indiana
Overall rating: 4 out of 5 4 out of 5

This is my 2nd Toshiba. My 1st Satellite crashed. This WAS NOT a roblem with the laptop itself!!! For this reason, i purchased my 2nd Toshiba. This laptop is very fast, reliable and well built. I highly recommend this Laptop for the everyday/intermediate user. Gamers may want to upgrade.

Great Student Laptop

POSTED BY: Ron , Delray Beach,Fl
Overall rating: 4 out of 5 4 out of 5

I have to say I enjoy having this laptop thumbs up

Works today!.

POSTED BY: doris , Santa Maria, CA
Overall rating: 4 out of 5 4 out of 5

As I learn about this new little computer, it is getting better. I hope to learn the variety of "things" that can be done with it! How do you "select al"l and send a message to a group of friends and relatives??

Some problems

POSTED BY: elmo , huntsville, AL
Overall rating: 4 out of 5 4 out of 5

I like the keyboard on the 3000/3005 series better. It has a better feel for typing. Windows 7 takes too long to initialize. Vista on the 3000/3005 series is quicker. Otherwise, I like this model very much and I am glad I purchased it.

first laptop

POSTED BY: campy , Pa.
Overall rating: 4 out of 5 4 out of 5

First time laptop user it's fine. the only trouble I have is seeing the keys when the light is bad.The battery dose not seem to last any where near the 5 hour they tell you.But I'm always near a receptical. I like it so far.

Great machine for the price

POSTED BY: pickles , wisconsin
Overall rating: 4 out of 5 4 out of 5

Had a toshiba laptop before this and was satisfied. Just wanted to upgrade and so far very satisfied.

I Love My Toshiba Satellite laptop

POSTED BY: parrk , Longview,Tx.
Overall rating: 4 out of 5 4 out of 5

It has so many features that no other computer or laptop has.Some were kind of hard to find,but all I had to do was call Toshiba and they just told me how to find any of the applications,and the battery life is so long I can use it almost along day without charging it.

Basically good

POSTED BY: dmicha , Swanton, OH
Overall rating: 4 out of 5 4 out of 5

I like the laptop itself but a tad disappointed in the speaker system to watch movies. I have tried hooking speakers up to the unit and the sound is even lower. Otherwise it is a great computer

Seems good...too early to tell

POSTED BY: RePete , North Fort Myers, Fl
Overall rating: 4 out of 5 4 out of 5

I like the way it works so far. Since I did not receive any owners manuel or operation manuel with purchase, I have no idea what it can do or how to do it. I am slowly learning on my own by experimentation. Seems fine..

Good or Solid Laptop

POSTED BY: Todd , Jacksonville, FL
Overall rating: 4 out of 5 4 out of 5

I think it is very portable as I could hook up the HDMI to my bedroom TV. I also could work at my kitchen table. The DVDs all worked. The movies worked good. It is good for Windows 7 and Wireless printers. The Wifi worked very well. Word 2010 is very good too. I also can hook up a Blu Ray Drive.

It's is ok

POSTED BY: vanny
Overall rating: 4 out of 5 4 out of 5

The speakers are very low

Decent

POSTED BY: EEarth
Overall rating: 4 out of 5 4 out of 5

Having gamma problems with monitor...but otherwise, it's a great computer:)

Good performance

POSTED BY: jule , la
Overall rating: 4 out of 5 4 out of 5

dislikes: usb plug in where you would use a mouse hard to click and drag hard to highlight touch pad hard to get used to short battery life, something like two hours

Works well

POSTED BY: Louis , Milwaukee WI
Overall rating: 4 out of 5 4 out of 5

Everthing is as advertized expect battery life. Only getting 3 hrs max instead of the 5 claimed.

Toshiba is my laptop of choice

POSTED BY: Alene , Tulsa, OK
Overall rating: 4 out of 5 4 out of 5

This is the 3rd Toshiba that I have owned and have always appreciated stability of the company and have always liked the performance of the laptop.

Toshiba Laptop rates very good

POSTED BY: Hos , Miami, FL
Overall rating: 4 out of 5 4 out of 5

Although I have not had my Toshiba laptop very long, it has been very reliable. Compared to my last laptop (not a Toshiba) the battery life is excellent. I hope the battery has a long life. My only complaint is manipulating whether I'm using wireless or ethernet, the network and sharing center software is a little confusing and took me a while to figure out.

One of the better lap tops I have owned

POSTED BY: gene , Georgia
Overall rating: 4 out of 5 4 out of 5

So Far, Very Happy.

POSTED BY: Dot , Houston, TX
Overall rating: 4 out of 5 4 out of 5

So far I'm very pleased with the performance and battery life of my Satellite L755-S5246 Laptop. But the true test is the durability. Will my laptop still perform well with no hardware issues 3 years from now? Anything less would negate this favorable review.

Excellent Value

POSTED BY: pirate , NC
Overall rating: 4 out of 5 4 out of 5

Start up time is good as compared to 1st gen i-core.Battery is improving with use. Like the positive feel keyboard. Touch pad is jumpy. Really need to add a wireless mouse, then smooth.

not bad for the money but no cigar

POSTED BY: Queens lawyer , delray beach, florida
Overall rating: 4 out of 5 4 out of 5

the pages shift without warning and not on command...the size of the font changes by itself...pages are lost without rhyme or reason and require re-starting the machine to recover them

Speakers

POSTED BY: Jeff
Overall rating: 4 out of 5 4 out of 5

The feature I don't like is the speakers and speaker volume. They're aren't loud enough and the quality is less then acceptable.....

MouseBad

POSTED BY: JohndbOne , Oklahoma
Overall rating: 3 out of 5 3 out of 5

Great laptop in every way except the mouse pad. Sometimes, no matter where or how I tap, the thing won't respond. Sometimes, no matter how or where I slide my finger, cursor won't move. This is not the first laptop I have had. To me this is a significant problem - it really cuts into productivity. You can say, "just buy a conventional mouse for it." But, then it's not a laptop any more is it?

goog laptop

POSTED BY: Chini , FL
Overall rating: 3 out of 5 3 out of 5

Some toshiba program slow down the pc, I had to uninstall them.

Good Buy

POSTED BY: Nickname , Silver Spring, MD
Overall rating: 3 out of 5 3 out of 5

Old (10 yrs.) desktop crashed, this was on sale at Office Depot and it was wife approved (Consumer Reports likes Toshiba), so I bought it. The main thing is it works.

midlevel

POSTED BY: poo , Tallahassee, FL
Overall rating: 3 out of 5 3 out of 5

Not fast enough.

good laptop if had windows XP

POSTED BY: Pineapple , Denver,CO
Overall rating: 2 out of 5 2 out of 5

most prograns i use do not work good with windows 7

satellite not so great

POSTED BY: Rhonda , Richland Wa
Overall rating: 1 out of 5 1 out of 5

freezes constantly battery life half of what it states.Have to pop out battery to reset.Slow ..hate windows 7

MSRP: $509.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Pentium® Processor B940
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories