Satellite L755-S5280 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best Value Laptop

POSTED BY: Psychologist , Upstate New York
Overall rating: 5 out of 5 5 out of 5

After a very disappointing experience ordering a laptop with a useless trackpad from another big name company, I went to the local big box store to actually see and feel the laptops. Keyboard layout is important to me since I have used the same layout for nine years and my fingers know where the keys and auxiliary/navigation buttons are “supposed” to be, and the trackpad is essential for my navigation of documents and the internet. Of course, I also need a computer that will handle the basics of word processing, digital images, Skype video-calling, web surfing and some large file transfers. This computer has the perfect layout for me, with a full-size keyboard and large enough navigation buttons to easily get around documents. Most importantly, the trackpad is a dream come true – it is flawless every time I touch it. You can spend thousands of dollars more and not get an experience as good as this laptop offers. It starts very fast, handles multiple tasks easily, and conserves energy without leaving me squinting to see documents. The screen is bright and crisp and high definition photos and videos display perfectly. The built in webcam is great and Skype calls operate smoothly. I am totally impressed. So why not a perfect five star rating on every item? Well, I would have liked a built-in modem (I still use a phone line for backup internet access) and the face-recognition security feature is also pretty lame – it will always be faster to type in a password to unlock the computer. I consider those two points pretty minor. This computer is a a terrific value.

Great value

POSTED BY: JOJO , Memphis, TN
Overall rating: 5 out of 5 5 out of 5

I really like having this new laptop

I love my Laptop!

POSTED BY: Wally , Vega Baja, PR
Overall rating: 5 out of 5 5 out of 5

Very good value

POSTED BY: H
Overall rating: 4 out of 5 4 out of 5

The cost performance ratio of the product is very good. It contains features that performance based rather than add-on based. I also like the smooth finish on the keys of the keyboard. The touch of the keyboard is also quite good.

CB's Satellite

POSTED BY: cgborboa , Hayward, CA
Overall rating: 4 out of 5 4 out of 5

Love the speed, features, size, weight, looks. There's a lot packed into this full-keyboard laptop.

good quality

POSTED BY: dalek , McCall, ID
Overall rating: 4 out of 5 4 out of 5

Yes I've owned a Toshiba laptop before and really liked it. This one is even better and it also has an HDMI port with is fantastic for streaming video off the net. One of my friends has also bought this laptop and she loves it.

POSTED BY: Bill , Ohio
Overall rating: 4 out of 5 4 out of 5

This is my second Toshiba Laptop. My first one is 10 years old and has been excellent. Bought a new one for increased capacity and speed. I anticipate the new one to be as durable as the older one. One design feature prevents me from giving the L755 an excellent rating: Location of the USB and other ports on the sides of the computer are in the way. Ports on the rear of the side and back of the computer do not interfer with operation. Ports on the side, toward the front are in the way, I am concerned that over time the ports could be damaged, plus the cables interfer with using the mouse, etc. Is there an L-shaped, compact conector available to route the cables to the rear of the desk? Thank you for requesting a review.

Very good laptop

POSTED BY: Artie , Farmingdale,NY
Overall rating: 4 out of 5 4 out of 5

Second laptop I've owned and I think it's great and easy to use. Would be nice to have a vulume control on the keyboard.

Excellent laptop for the money

POSTED BY: CGB - Satellite , Hayward, CA
Overall rating: 4 out of 5 4 out of 5

Excellent features, speed, size and weight.

Toshiba Laptop Review

POSTED BY: Chino , Jax, Florida
Overall rating: 4 out of 5 4 out of 5

This is my second Toshiba Laptop. Overall satisfied with it. As of this review the only two cons I will note are as follows;Keyboard keys feel cheap; and the speakers aren't very good. Otherwise function, style and software are good enough for me.

Very good computer for students

POSTED BY: Geo , Los Angeles
Overall rating: 4 out of 5 4 out of 5

This laptop is mostly used by elementary students in the home. It feels less flimsy than Lenovo, Acer and Asus. It is much, much more reliable than Lenovo and HP; I never had a problem with any of the 3 Toshiba laptops I purchased. Overall, it is a great performer for the price paid.

MSRP: $521.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2310M processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories