Satellite L755-S5311 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Fantastic

POSTED BY: Drew , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

This is an awesome laptop perfect for both gaming and visuals. Also, it is good for media Speakers are great Picture is crisp.

Great Laptop!

POSTED BY: rceckspurt13 , Olalla, WA
Overall rating: 5 out of 5 5 out of 5

There are so many things to love about this laptop. First is the battery life. the battery easily lasts a few hours, even under heavy processor loads such as 3D gaming or watching and editing videos. When fully charged, it easily lasts me the majority of a day under normal use (ie. web browsing). The Core i3 processor. This thing is fast! It has easily handled everything I could throw at it; Games, video, and multitasking. I haven't had any slowdowns whatsoever. Heat is another thing that this laptop handles better than others. This laptop runs extremely cool, even at high processor loads. I've only gotten it to feel slightly warm to the touch even after a full day of gaming. The screen is bright and crisp. the LEDs are a big improvement over a standard backlight by cutting out warming up time. The speakers are loud enough and sound pretty good for a laptop. The only thing I wish it had was a backlit keyboard to make working in low light easier. However, none of my other laptops have had this, so it isn't a major hinderance. Overall, this is a great laptop for the money. You will get power, convenience, and quality all rolled up into one package. You cant go wrong with this.

Fast,Fun,Fantastic

POSTED BY: pop pop , port st. lucie
Overall rating: 5 out of 5 5 out of 5

This computer is what I have been looking for. 4gigs of ram exspand to 8 .Great battery life, 10 pad key pad,camera,mic, the works best part all this punch and only 5lbs.

great value computer

POSTED BY: pjabru , NY
Overall rating: 5 out of 5 5 out of 5

I needed a new laptop computer and wanted a Intel i3 processor. The price was great and very happy with the performance.

Great Value!

POSTED BY: R & J , Mishawaka, IN
Overall rating: 5 out of 5 5 out of 5

Bought this laptop one month ago and couldn't be happier. I mostly use it for light tasks and web but also edit photos using Adobe Photoshop Lightroom 3. I can edit and add multiple adjustment layers with no drop in performance. I have the 4GB RAM model and my performance widget usually has the RAM at about 50% usage. If you are going to do serious multi-tasking would recommend RAM upgrade to 8GB.

best laptop i have own

POSTED BY: sissy , asheville,nc
Overall rating: 5 out of 5 5 out of 5

i love my laptop that i received as a christmas gift. very easy 2 manvuer & very user friendly.

Sleek design

POSTED BY: Paintbrush , Allentown PA
Overall rating: 5 out of 5 5 out of 5

Great laptop, easy to store, easy to carry and easy to operate, this was a great gift.

Best Laptop Ever!

POSTED BY: merfmommy , buffalo ny
Overall rating: 5 out of 5 5 out of 5

My first Toshiba laptop was great. This new machine is 100 times better. Thank you Toshiba.

So far, so great!

POSTED BY: Earthstar , Lutz, FL
Overall rating: 5 out of 5 5 out of 5

Great value for the money. Highly functional, many features, feels great in your hands, is very quick, great price. We are really pleased.

Very happy with my purchase

POSTED BY: Dex , NW Washington
Overall rating: 5 out of 5 5 out of 5

I got this laptop on New Year's Day and it is one of the best deals I have gotten. All my friends are quite impressed with it. It has everything I was looking for when shopping for a new laptop and I love Toshiba products. And the apps and features it comes with are nice little extras. I use it mainly for photo editing and Microsoft Office and it purrs along very smoothly. I really don't think I could have gotten a better product for the price.

I love this laptop!

POSTED BY: wolverinelover1011 , Toledo, Ohio
Overall rating: 5 out of 5 5 out of 5

i love the price, how well it works, how long the battery lasts. The size of the laptop is great.

Completely satisfied

POSTED BY: Steve , Somerset, NJ
Overall rating: 5 out of 5 5 out of 5

Purchased this laptop to browse the web, email, etc. Have used Dell and Hp in the past and Toshiba has far outperformed them both.

so far so good

POSTED BY: vic , middletown, de
Overall rating: 5 out of 5 5 out of 5

so far sogood, i have had my laptop for a month and am happy with it,

Great laptop for the price!

POSTED BY: UMOStudent , Bangor, ME
Overall rating: 5 out of 5 5 out of 5

I have had this laptop for a little over a month now, and I must say that I'm extremely impressed! This laptop offers so many features and the quality is impeccable for the very modest price tag. I would recommend this to anyone who is a student or needs a laptop for personal use.

Toshiba review

POSTED BY: KL , St Pete, F:
Overall rating: 4 out of 5 4 out of 5

I like the new computer; nice keyboard, easy to read features. Batterylife is NOT what I expected.

Good Value

POSTED BY: Tosh.11
Overall rating: 4 out of 5 4 out of 5

My computer has the basic features at a reasonable price.Since I've only had it for over a month I'm still learning more about it.

full number pad

POSTED BY: akgirl , anchorage,ak
Overall rating: 4 out of 5 4 out of 5

because of the work i do i need a laptop will a separate num key pad this laptop is the perfect size!!

Great

POSTED BY: terwilwc
Overall rating: 4 out of 5 4 out of 5

This laptop is great. I use mine as my desktop with my large monitor and wireless keyboard and mouse. It could use an additional USB port, but otherwise it's a great laptop for the money.

Wonderful!

POSTED BY: Worm , Amelia, Ohio
Overall rating: 4 out of 5 4 out of 5

Love my new laptop! This is the third Toshiba are family has bought in the last year. And so far they are a great laptop.

Good laptop for the price

POSTED BY: buckeye , Cincinnati OH
Overall rating: 4 out of 5 4 out of 5

However, it is the worse mouse touch pad I have ever had on any laptop.

Reasonable product for the $

POSTED BY: LP Investigator , South Dakota
Overall rating: 4 out of 5 4 out of 5

Overall I am satisfied with the product. Pro's- I like the scroll functions on the touch pad. I also like the quick button above the scroll pad to shut it off. The keyboard layout is good. I don't feel cramped as I sometimes do while typing with other 15.6 laptops. The connections are ample: 3 USB ports, an HDMI and a VGA. Con's- Battery life is relatively short, but pretty standard for this price point. The sound system is also lacking. My Fiancee purchased a laptop at the same time from another company and has much better sound (spent $90 less than me). Overall I cannot complain for the price. With regards to the battery, the laptop comes with Eco-mode software that helps you maximize battery life while minimizing power consumption. As far as the speakers are concerned, the only time I really want decent sound out of my laptop I am either going to be wearing headphones or will plug into an external speaker system.

Great Value but it has drawbacks.

POSTED BY: CriticalCritic , Cary, NC
Overall rating: 3 out of 5 3 out of 5

I love this laptop, but when evaluating any laptop, I compare it to my 4 year old Toshiba Satellite (My favorite of the 6 laptops that I have owned over the years). This laptop ranks in at second place overall for my laptops over time, adjusting for advances in technology of course. Like with any toshiba Satellite, this thing has some of the best laptop speakers on the market. The ports are intelligently laid out, and the stock Toshiba software is non-invasive. There's not much I could ask for with respect to the star ratings above. However, the reason that this laptop does not meet my expectations for a 5* laptop is that, plainly put, the keyboard is of sub-par quality in today's market. This feature, the main input on a laptop, terribly drives down the user experience. Of everything that i could desire in a device, that I will be typing on for hours on end, above all else I want a good screen and a great keyboard. well, this Toshiba has an excellent screen for the price, but the keyboard is abysmal at this price range. the keys are weak, wobbly, they twist, and they sometimes mis-key (the shift key is the worst for hitting but not registering). In addition, I've had this laptop for exactly one month and I am seeing a glare on most of the keys due to either the texture wearing off, or the high absorption of the oils from my fingertips (I'm not sure which it is). Either way, this is really not what i was expecting. finally, these problems are made worse by the fact that Toshiba doesn't seem to offer replacement keyboards for this model! And I can't do online chat with a representative because Toshiba apparently doesn't offer that service to customers. Well, on the bright side, the keys are relatively silent, and everything else is either of acceptable or superior quality.

POSTED BY: marketrsh , raleigh, nc
Overall rating: 1 out of 5 1 out of 5

had for two months and it wont boot. black screen. would not recommend. also mouse pad works poorly, this is the worst laptop i ever owned.

MSRP: $529.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-2330M processor
  • Windows 7 Home Premium (64-bit), SP1
  • 4GB DDR3 1333MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive

shop for accessories