Satellite L775D-S7220 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

A Good Computer

POSTED BY: ITdemon13 , Fort Knox, KY
Overall rating: 5 out of 5 5 out of 5

Toshiba is a good computer that is easy to use and is also great for users that are both Tech Savvy and those that are just starting to get into technology.

Nice work space

POSTED BY: Just me , Bellevue, Ne.
Overall rating: 5 out of 5 5 out of 5

I find this PC to be a great all in one machine. Performs all task I have ask of it, and plays my fav games to boot.

Best laptop I've ever had....

POSTED BY: Nette , Nashville, TN
Overall rating: 5 out of 5 5 out of 5

This is the best laptop I've ever had, and I like it so much I no longer use my desktop. The only thing I don't like is it's not loaded with Winddows XP, which is what I prefer. However, I will get used to it and wonder why I didn't switch sooner.

Laptop Problem

POSTED BY: Machan , Pensacola, Fl
Overall rating: 5 out of 5 5 out of 5

The laptop is a very nice computer. The ONLY Problem that I have with it, which you supposedly are already aware of is the clock gains three to six hours every day and requires re-setting everytime I use it.

System board Battery

POSTED BY: Bob , Fayetteville, NC
Overall rating: 5 out of 5 5 out of 5

I bought this PC and it kept looseing system time. the intrernal battery is bad. Qiuck response from the Support desk, I got the shipping box and label fast. Hope to get it back fast.

POSTED BY: Larry , Buffalo Wy
Overall rating: 5 out of 5 5 out of 5

A great machine so far but not perfect. I am having trouble with the internal clock. It keeps time while it is pluged in but when shut down and unpluged the clock runs at about 2X speed. Any help you could give would be appreciated. My wife and I purchased two of these units at the same time and her clock works fine so I know it can be done. Really like the screen size.

love this!!

POSTED BY: hpop , oxford, ms
Overall rating: 5 out of 5 5 out of 5

this is my second toshiba laptop and i love it!! the graphics are amazing and the price was right. the only problem is every time i turn it on i have to reset the clock. its aggravating but not really a big deal.

POSTED BY: Bob , US
Overall rating: 5 out of 5 5 out of 5

Just what we were looking for.

Clock issue

POSTED BY: Bill
Overall rating: 5 out of 5 5 out of 5

We bought this computer to replace our 8 year old HP. Never used a laptop before took some getting used to but now am very happy we got it. The only issue we have is with the clock as others have. After shut down it gains 12 hours over night. Took it to the place we bought it from and they are going to check into it. Otherwise we have no promblems with it.

Excellent

POSTED BY: ibeme , Kingman, Az
Overall rating: 5 out of 5 5 out of 5

I have used several brands of computers. This one so far has been the simplest to figure out. Fast response to anything I want it to do. I really enjoy using it.

Great Laptop

POSTED BY: Pete , Alexandria, Va
Overall rating: 5 out of 5 5 out of 5

I bought this laptop to replace a gateway and this is much superior to the gateway and others brands that I have tested at the retail stores. Great machine for the price.

Awesome Laptop

POSTED BY: Janie , San Antonio, TX
Overall rating: 5 out of 5 5 out of 5

I love this laptop, keyboard and screen are the perfect size but the laptop is not overly heavy and will be easy to take along when needed. We now have 3 Toshiba laptops in our home!

AMD & Toshiba #1!!!!!!!!

POSTED BY: wyruss , Ogden, Ut.
Overall rating: 5 out of 5 5 out of 5

I have been wanting a laptop for 20 yrs. and finally was able to choose the one I wanted. Only 2 requirements...Toshiba with an AMD chipset...THANK YOU....

A good buy.

POSTED BY: eml , Milwaikee, WI
Overall rating: 4 out of 5 4 out of 5

I reserched b/4 buying and discerned that this was the best quality offer. I use this as a portable office computer when I am on the road, to suppliment the many othe rcomputers at my disposal.

needs better quality control

POSTED BY: rebarns , Constable, NY
Overall rating: 3 out of 5 3 out of 5

Had laptop for a couple of weeks and harddrive has already went down.

MSRP: $599.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Dual-Core A4-3300M Accelerated Processor
  • Windows 7 Home Premium (64-bit)
  • 4GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)