Toshiba Satellite L855-S5138NR Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Totally Toshiba

POSTED BY: Insectman , WV
Overall rating: 5 out of 5 5 out of 5

I am on my 3rd Toshiba in about 15 years. My wife is on her second in about 10 years. We did not look at another brand when we bought our last one. The computers are great and the service is excellent.

Great Laptop

POSTED BY: Mom , Ohio
Overall rating: 5 out of 5 5 out of 5

I just replaced my Toshiba laptop after using the same one for 6 1/2 years. I loved it! I chose Toshiba again because I was satisfied with the reliability and ease of use of my old laptop. My old Toshiba made it through a bachelor's degree, still carries my master's thesis, my doctoral dissertation, yt dissertation defense presentation, over 100 lecture presentation, not to mention my music and photos. I never turned it on and had it not come right up. My husband has an HP that cost hundreds more, and he has had nothing but problems. My new laptop is working like a charm, as expected, as well. My only complaints are that the mouse pad does not work as well as my old one. Also, Windows 8 is a disappointments in some respects. Too many often used features are gone.

MSRP: $554.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3120M Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories