Toshiba Satellite L855-S5163 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great value and features

POSTED BY: Bob , Inland Empire, CA
Overall rating: 5 out of 5 5 out of 5

The Toshiba L855 has everything I wanted, and probably more than I'll need to use. I find this PC to be a very effective tool. I need to get more familiar with Win8, but I am very happy with this powerful feature-rich PC.

Nice Machine

POSTED BY: Bob , Bellaire,MI
Overall rating: 5 out of 5 5 out of 5

Had many laptops but this is really a great machine. Great screen, fast, easy to use

Good value

POSTED BY: God's Child , Granada Hills, CA
Overall rating: 5 out of 5 5 out of 5

It is fast and works well.

Purchased one just like my daughters

POSTED BY: new business , Finley CA
Overall rating: 5 out of 5 5 out of 5

I have had a few brands of computers but the Toshiba laptop we purchased 7 years ago is the only one that is ALWAYS working. My older daughter purchased a new Toshiba laptop with windows 8 for college and I liked it so much I purchased the same one for myself. I just love it!

Excellent performance

POSTED BY: Jay , Puerto Rico
Overall rating: 5 out of 5 5 out of 5

Very nice laptop with lots of features. Fast interface, great price.

Super fast laptop

POSTED BY: Roger , Vacaville, Ca
Overall rating: 5 out of 5 5 out of 5

This laptop is super fast with the CORE i7 processer and easy to use keyboard. It starts up in no time at all with no fuss. The new Windows took a little bit to get used to, but now I can navigate with no issues. I plan on using this laptop for mostly business use and it should be great with the Microsoft programs that came with it.

Love it

POSTED BY: Laptop fan , Connecticut
Overall rating: 4 out of 5 4 out of 5

Product so far is excellent value. The blue ray player is a great option and when hooked up with the HDMI cable to the large falt screen tv what an awesome picture. Windows 8 takes some getting use to but the Toshiba icon when clicked on you can use it like a desktop model with all your favorites

Great laptop

POSTED BY: Suezie Q , University Place, WA
Overall rating: 4 out of 5 4 out of 5

I am very satisfied with my purchase. I love the keypad feature.

Very disappointing performance

POSTED BY: Herbert , NorCal
Overall rating: 3 out of 5 3 out of 5

Beautiful keyboard layout (numpad!), but keyboard seems to flex as you press, which is a bit unnerving. Compared to other i7-based PCs, THIS THING IS SLOW. Sure wish I could recommend it.

Toshiba Satellite

POSTED BY: John , Dallas Texas
Overall rating: 2 out of 5 2 out of 5

Should be offered with Windows 7 Mouse finger pad is often unresponsive for up to 25 seconds Space bar is too small - when using the space bar I hit the Alt or other keys - I lose a lot of data because of this. The back space key is not like my other keyboards. I will return this machine as soon as I can find a high performance machine with Win7.

Windows 8

POSTED BY: Larry , Ca
Overall rating: 1 out of 5 1 out of 5

I disliked windows 8 so much I returned the computer. I will switch to Apple before I go back to anything that resembles Windows 8.

MSRP: $935.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-3630QM Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750GB (5400rpm, Serial ATA)
  • Blu-ray Disc™ ROM (BD-ROM) and DVD SuperMulti drive (+/-R double layer)

shop for accessories