Toshiba Satellite L855-S5187 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Best Quality Laptop Bought

POSTED BY: JImbo , NJ
Overall rating: 5 out of 5 5 out of 5

Easy setup,Quality ,fast CPU, Light ,all the functions you would need in a laptop

Windows 8 really is bad

POSTED BY: Pat , San Jose, CA
Overall rating: 4 out of 5 4 out of 5

The computer is just fine but the windows 8 portion of the system really sucks! It is just confusing especially since I have no need for all the social media junk that is up front and in my face.

Very fast processor

POSTED BY: pdxuser , Portland, Oregon
Overall rating: 4 out of 5 4 out of 5

I needed a fast processor for an application building project, and my older computer was just way too slow. The i7 processor is very fast and most applications on this laptop open in a blink. For example, pages on Internet Explorer and my mail program open as fast as I click. Great! And my other slow apps now work at blazing speeds. No problem with waiting anymore! I did a lot of research before buying. I wanted a 15.6 computer with high resolution and i7 (full speed - not U), and a touch screen, but no one is making touch screens with a full i7 processor yet - maybe fall of 2013. So this was the best compromise till they do - and at a great price point. basically - everything works as advertised, and the machine is solid.

MSRP: $709.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i7-3630QM Processor
  • Windows 8
  • 8GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories