Toshiba Satellite L875-S7153 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Toshiba-PC

POSTED BY: aleksasha , Middletown NY
Overall rating: 5 out of 5 5 out of 5

I believe that the computer is a very good light shows. I bought a computer for myself and a few days later bought the same model for a father. We are very happy. Thank you.

review for Toshiba Satellite laptop

POSTED BY: johno , Boulder, CO
Overall rating: 3 out of 5 3 out of 5

TOSHIBA Satellite L875-S7153 I bought this based on reviews and needing to upgrade to something more modern. The machine is very fast, tons of ram and HD space, and the screen has great resolution. The main 3 drawback are: 1. within a few days, the right half of the screen appeared on the left, and the left was on the right. I was able to fix (for now) using an updated driver from AMD, but not sure if that problem will return (I was lucky to find this "fix" as most consumers would probably have to just send it back). 2. just comparing this laptop to my previous one (which still works after 9 years), it looks pretty much impossible to work on (replace a keyboard or screen). This bothers me, as I don't believe a computer should be a disposable item to be replaced with another one. It should last for years and like a car, should be able to have periodic hardware maintenance performed - as needed - but that may be just the way all laptops are going. 3. The speakers aren't very good (weak, not very crisp/clear sound). Not a fan of Windows 8, but that's a separate issue not related to the machine.

MSRP: $699.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i5-3230M Processor
  • Windows 8
  • 2GB DDR3 AMD Radeon™ HD 7670M Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)
  • Wi-Fi® Wireless networking (802.11b/g/n)

shop for accessories