Toshiba Satellite L875D-S7342 Laptop

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Very nice combination of speed, graphics and price

POSTED BY: RadioFlyer , Halifax, Pa.
Overall rating: 5 out of 5 5 out of 5

This laptop has excellent graphics for editing photos in hi-resolution. It's processor can easily perform several functions at the same time without affecting speed. The DVD multi-disc drive works very well not only in showing movies but also burning disks. I am quite satisfied with the features and performance of this laptop and glad I purchased it.

my lapton

POSTED BY: xboxgrandpa , East Hampton,CT
Overall rating: 5 out of 5 5 out of 5

I've had good luck with my Toshiba laptops. I like how they don't get real hot. like windows 8 on my new one.

Very nice computer.

POSTED BY: MamaLinda , Myrtle Beach SC
Overall rating: 5 out of 5 5 out of 5

I looked for over a year for a replacement for my Acer laptop, which worked just fine and I gave to an elderly friend, and tried several All in One systems, but none seemed right. I think I was just too used to laptop system. Anywho, my son and his wife both have had their Toshiba's for several years w/little trouble and the specs on this were very impressive to him, he's a techie, so I finally bought. I love being able to go back and forth between Win 8 and traditional Win 7 screens. I had no problems learning Win 8, I like to play around and am not afraid of computers. I also have a Mac Pro 1 yr old that was my late daughters' and its IOS gives me fits and I can't play my silly games on it properly. This is fast, lots of memory and fun to see all it can do. (I am still learning). All in all a very nice system, would recommend , and wish I could have gotten it in Red! 4 stars on performance and battery only because I haven't tested battery yet and don't know all this beast can accomplish! Enjoy.

Excellent product

POSTED BY: SFL , Florida
Overall rating: 5 out of 5 5 out of 5

I love my new laptop. I replaced an old one that quit working. The windows 8 was a bit of a challenge at first since I was using Vista but soon got the hang of it. The price was very good for the amount of options that are offered on this machine. The keyboard size is excellent no crowding of letters together and typing feels very natural. I find the colors very clean and sharp for the everyday user. It runs quiet . My only complaint is that I would have liked to have been given a written quick start instruction manual. The on screen manual is not helpful if you are just getting acquainted out of the box. Thankfully, this was not my first computer so I had a bit of knowledge to fall back on. But like I said the windows 8 was a bit scary at first and a manual would have helped me feel a bit more secure just starting out.

Great Laptop

POSTED BY: jbigmoneygrip , NC
Overall rating: 5 out of 5 5 out of 5

I found this laptop to be very good. It was easy to set-up and everything you needed is right here at your fingertips and luv windows 8

Love Toshiba

POSTED BY: mygonc , Fresno, CA
Overall rating: 5 out of 5 5 out of 5

This computer is great. I love the bigger screen.

Laptop

POSTED BY: Jackie , Laurel,Ms.
Overall rating: 5 out of 5 5 out of 5

So far my laptop is great. I don't do a lot on the internet, but what I do is enough.

Second Toshiba-really pleased

POSTED BY: Granny , Terry, MS
Overall rating: 5 out of 5 5 out of 5

The only thing that has been a little difficult is learning Windows 8. Otherwise the computer performs beautifully.

Best laptop that I have ever owned.

POSTED BY: john , Waymart Pa.
Overall rating: 5 out of 5 5 out of 5

I am familiar with Satellites. Like big screen. Like Win 8. Very easy to use. My family likes my new computer. Would recommend to a friend.

POSTED BY: John , Niceville, FL
Overall rating: 4 out of 5 4 out of 5

I was hoping it would come with Windows 7 installed. I'm not sure that I like Windows 8. Since I do not have the touch screen, it's a little difficult to use with the mouse pad. Even with a regular mouse attached, it is still difficult to use. I really do not like the idea that all the extra software comes preloaded: i.e. Norton software. I have additional software that I use and have to uninstall the other stuff. If you left all the extra software off, the price could be less. I would like to have a copy of Windows 8 come with the computer. Several times, I have been infected with a virus and had to reformat the hard drive to get rid of it. That is hard to do without the disk. I know that a boot disk can be made, but that is an extra burden on me. It seems that the computer manufacturers are trying to cut corners by not including the disks

laptop

POSTED BY: lou , Murfreesboro,Tn.
Overall rating: 4 out of 5 4 out of 5

like computer just not sure about windows 8. I am not computer savy so harder for me.

touchy screen

POSTED BY: Sherry , marietta ga
Overall rating: 4 out of 5 4 out of 5

This screen is so touchy it jumps you right out of your site with the least possible provocation. Barely moving the cursor will take you to the sign out page or the home page or any other danged page it wants too. Trying to close a window or get the cursor to respond in the corners is also mostly impossible. I am totally not pleased with the touchiness of this. Maybe this is a windows 8 problem and not the computer. I am not loving windows eight either.

Might I Be Stupid?

POSTED BY: Roro , South Florida
Overall rating: 4 out of 5 4 out of 5

I bought this laptop because my previous one had died after only 4 years. That laptop was also a Toshiba Satellite. I'm hoping this one lasts longer. If not, I guarantee this will be my last Toshiba!

Laptop Excellant, Configuration poor

POSTED BY: Chem9 , Roanoke, VA
Overall rating: 2 out of 5 2 out of 5

Laptop was very good in comparison with competitors, However Toshiba used a bios configuration that was not user adjustable for virtualization when upgrading software to Windows 8 Pro in order to use Hyper-V function without paying Toshiba to turn the switch on. All competitors allow user to change bios setting. Having to pay extra for this caused me to return the computer back to seller. Toshiba used to be great.

Not impressed but good price

POSTED BY: notageek , raytown, mo
Overall rating: 2 out of 5 2 out of 5

Good price but not very impressed. Nice size, glad it has 10-key but keys are cheap quality to the touch making typing not as easy as it should be. Very stiff, thin and hard feeling...not very flexible for the average user. Don't know why laptop makers are switching to this type of key..very cheap quality. Do like the feature of the many USB ports.

bought a lemon

POSTED BY: ptrepete , richmond, tx
Overall rating: 1 out of 5 1 out of 5

Nothing works on this laptop. I cannot get passed sign in without it freezing up. Tried to download Toshiba for dummies and all I got were blank pages. I rated it a 1 only because there was no 0.

MSRP: $629.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A8-4500M Accelerated Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • AMD® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories