Toshiba L955-S5142NR Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Nice Lap Top

POSTED BY: Ray , Winter Garden Fl
Overall rating: 5 out of 5 5 out of 5

This is my second Toshiba and I loved the first one,it to was a Satellite. Well I got a lot of years from it and wanted to stay with Toshiba. I ordered my L955 from a retailer on line and could not wait till it came. The new L955 S5142NR is so fast it has then what I need in features. The new windows 8 was a bit for me for I was using windows Vista. After a day or so I really started to like it. My L955 came with 6gb of Ram and a 630 GB hard drive. I run a lot of programs and needed something that I could do that and this Lap Top dose it with ease. I am already tell my friends that are thinking about replacing there old Lap Top to go with the Toshiba for the long term they will take all the run time and still preform. Thanks Toshiba for staying on top of the list.

Great laotop!

POSTED BY: Willie , Clovis, Ca.
Overall rating: 5 out of 5 5 out of 5

I love the computer....the screen, the quick it boots up & down. Also the battery life has improved over my last one. I am still trying to understand Windows 8. this may take some time. Any help with this would be appreciated. Thanks for another great laptop.

best so far! hehe

POSTED BY: zhogs , Calamba, Laguna Ph
Overall rating: 4 out of 5 4 out of 5

my 2nd laptop and better compare to Dell.. hehe

POSTED BY: Jacky , Bayamon, PR
Overall rating: 4 out of 5 4 out of 5

I love the keyboard, i would recommend screen should be more wide. Resolution is perfect. Good cache and I love to have more than 500 GB of hard disk. For me this model of toshiba is a great computer.

MSRP: $574.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3227U Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories