Toshiba Satellite L955-S5362 Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Great Laptop

POSTED BY: LEO , PR
Overall rating: 5 out of 5 5 out of 5

I like the laptop very much. Its fast and easy to use.

Fast Laptop

POSTED BY: Span , Lewisville,Texas
Overall rating: 5 out of 5 5 out of 5

I am quite pleased with my new toshiba Intel I-3 laptop. It's fast , exactly what I wanted in a laptop as far as features. I would highly recommend this laptop to friends and family!

First personal Lap-Top

POSTED BY: Bill , Temple, Texas
Overall rating: 5 out of 5 5 out of 5

Easly replaced my Desktop with many more features.

Skeptical but pleased

POSTED BY: WyoWalt , Sheridan, WY
Overall rating: 5 out of 5 5 out of 5

I was very skeptical about buying a Toshiba but must admit after 30 days I am very pleased. It is very fast. I do use an external mouse as I do not like touch pads and the one on this laptop does not function all that well.

its light and sweet

POSTED BY: madgamer , san antonio, tx.
Overall rating: 5 out of 5 5 out of 5

very lightweight and sleek nice design the color could have more choices. the features r good some r needed more than others could have done without some the battery is the best not quite 6 hrs but compared to my last laptop gateway its exceeds all expectations. one issue why are the original games freecell, solitare.etc not on cpu

Love it!

POSTED BY: Snoozy
Overall rating: 5 out of 5 5 out of 5

A really great product!!

Best Laptop Ever!

POSTED BY: SuperStar , Los Angeles, CA
Overall rating: 5 out of 5 5 out of 5

My Toshiba Satellite L955-S5362 Laptop is light-weight, stylish, and processes very fast.

Great value

POSTED BY: aldese , NM
Overall rating: 4 out of 5 4 out of 5

The computer itself is fantastic but I would like to get rid of Windows 8. I am a grad student and have used Windows OS throughout my education and career so I believe I am a proficient user. I have yet to figure out how to keep the screens from switching over and I also can't figure out how to get a program like skype off the app list and onto my desktop. This is a very annoying OS.

Very Happy with my new laptop

POSTED BY: Tony , Westport Ma
Overall rating: 4 out of 5 4 out of 5

Best laptop I ever use

ToshibaL955

POSTED BY: Sonny , New Jersey
Overall rating: 4 out of 5 4 out of 5

I have an older Toshiba Satellite computer which served me very well.I decided to upgrade to the newest technology.

easy to use for beginner

POSTED BY: Red , St. Louis, Mo
Overall rating: 4 out of 5 4 out of 5

I am not a daily user of the computer or the vast features it has to offer (like the apps) and found this easy to learn and navigate. Each time I turn it on I learn something new.

Laptop Review

POSTED BY: Guitar man , Michiana area, IN
Overall rating: 4 out of 5 4 out of 5

The keyboard and function keys are very well laid out for someone with large hands. The screen is very clear and has great color. Sound is very good. Not real happy with Windows 8 when running software, Software purchased last year (Pro Tools) has compatibility problems. This is my third Toshiba laptop and would recommend to my friends and family

first laptop

POSTED BY: wacker , lockport ny
Overall rating: 4 out of 5 4 out of 5

still learning but enjoying it

Some Problems

POSTED BY: serving , South Dakota
Overall rating: 3 out of 5 3 out of 5

I like the Toshiba, however I have had a couple of problems. The keys don't always type the letter; sometimes takes 5 or more times of pressing it or just waiting for a couple of seconds (0-15) Sometimes it starts to type in caps and the light on the key isn't lit and pressing it doesn't revert back to normal type pattern. it's happened each time I'm working on a document. It also switches size of the page--like 100% to 25% or 70% to 150%. It's frustrating

Nice but frustrating

POSTED BY: Mac , Colordo
Overall rating: 3 out of 5 3 out of 5

I enjoy the size and weight of this computer, but HATE Windows 8. Have only had this laptop a few weeks and fnd the keyboard unreliable....it skips letters unless you press each one hard or it doubles a letter. Had to buy a wireless keyboard just to function without going back to correct words. Am not used to screens moving around and have had issues with Internet connections. The mouse cursor is all over the place and disappears often. I hope it is merely a matter of getting used to a new computer. It does have good battery life, but I prefer the older OS and something I am familiar with. Was disappointed I had to load some card games and this comes with no Office, Word, etc. Mouse pad clicks loudly!!! In time I will adjust to the quirks, but I wish Microsoft would leave well enough alone and stay with an OS longer than they do!!

to early for review

POSTED BY: vaille , fort lauderdale, fl
Overall rating: 3 out of 5 3 out of 5

I think it to early I just bought my laptop for me a review should be done at least after one year

POSTED BY: dreamlady1931 , Alexandria MN
Overall rating: 2 out of 5 2 out of 5

too hard to switch over to, after a month have too many glitches that take too much time to solve or just have to deal with.

Hate the keyboard

POSTED BY: Kim , Oswego, IL
Overall rating: 2 out of 5 2 out of 5

I love my new computer. I hate the keyboard. You have to press hard to make the key strokes. Would not buy one like this again. It's terrible. Always making corrections, etc..

windows 8 disappointment

POSTED BY: spacewick , St Thomas, VI
Overall rating: 2 out of 5 2 out of 5

Laptops nice but windows 8 is garbage. Very cumbersome. Makes you reopen windows frequently and battery life is shorter because new system leaves to much running in the background.

Surprisingly disappointed

POSTED BY: dmoe , Glendale, az
Overall rating: 2 out of 5 2 out of 5

I did a lot of research on laptops and came to the conclusion that the satellite was the one for me? After 1 month my keyboard went out and haven't yet been able to get it fixed due to my needing it for school, so I had to go out and buy a wireless keyboard to complete assignments and that has been a pain in the booty.

MSRP: $649.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™ i3-3217U Processor
  • Windows 8
  • 6GB DDR3 1600MHz memory
  • Intel® Integrated Graphics
  • 750 GB (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories