Toshiba Satellite L955D-S5140NR Laptop

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Toshiba Satellite

POSTED BY: lee , Spring Lake, MI
Overall rating: 5 out of 5 5 out of 5

Awesome computer. I loved the satellite laptops so much I bought my second one. Love how fast it wakes up and connects to the internet. Will be a Toshiba buyer forever.

Disappointed-Definitely not worth the price

POSTED BY: student14
Overall rating: 2 out of 5 2 out of 5

This is my 3rd Toshiba laptop. I have been very happy with my previous Toshiba satellite laptops. This one however, I am very disappointed in. It is SO slow, I often have to reload pages because they will just keep on spinning. I only use my computer for school, and web browsing, so no games. It can barely keep up which is very frustrating. I thought that with the quad core processor it would be fast, but no. My baseline model that was 3+ ears old performed much better. I would expect pay no more than $300 for a computer that performs so slowly which is why I did not and bought what I thought was going to be a new and fast, trusted computer. This computer also just feels cheap and the keyboard is terrible and not user friendly at all. Unfortunately, I had to order it online and needed it urgently for school as my other one broke. I did not have the option to return it for something different; if I could, I would in a second. I am hoping I can keep my sanity and can limp this one along until I am done with school and upgrade asap.

MSRP: $554.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Quad-Core A8-4555M Accelerated Processor
  • Windows 8
  • 6GB DDR3 1333MHz memory
  • AMD® Integrated Graphics
  • 640GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti drive (+/-R double layer)

shop for accessories