Satellite M305D-S4833

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Fantastic Laptop

POSTED BY: Sarah , Colonial Heights, Virginia
Overall rating: 5 out of 5 5 out of 5

I got this laptop for college. This laptop is fantastic. It's very fast, even when loading up from being turned off. My boyfriend has a Sony Vaio and this is way better, he often tells me he's jealous of it. It comes with a great webcam, facial recognation instead of using passwords, built-in FM radio that sounds great, and AWESOME Harmon/Kardon speakers. The only things I don't like about it is "Fusion Finish" fingerprints are EVERYWHERE, but that problem is easily fixed with the cleaning cloth Toshiba provides, and I think this laptop is rather heavy. This computer works perfectly on our wireless network, including a wireless printer. I love it and I HIGHLY reccomend it.

great performance and mobility

POSTED BY: LOS , charlottesville,va
Overall rating: 5 out of 5 5 out of 5

i am not a very sufficient computer user , but this laptop has definately helped with getting me further along with what i need to know. this is a great laptop- very lightweight, easy to use and pretty secure when it comes to the internet. i will give it a 9.5 out of 10!!!

best laptop ever inmy hands

Overall rating: 5 out of 5 5 out of 5

this is a very good laptop.wont buy anyother fastthinlight weight good sound grafics everything

MSRP: $899.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ X2 Dual-Core Mobile Processor RM-70
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless LAN (802.11b/g)

shop for accessories