Toshiba Satellite NB15T-A1302 Laptop

Average Customer Rating:
up to $50 OFF Microsoft Office

Limit 5 per household

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

Excellent

POSTED BY: zakousky9 , Humacao, PR
Overall rating: 5 out of 5 5 out of 5

I buy this laptop for my mother, she is a teacher, she usually uses office, facebook, teacher software. You can use the laptop like a tablet or like a computer and is very portable. She really like it.

Great Value for the Price

POSTED BY: dfs95819 , Sacraemento, CA
Overall rating: 5 out of 5 5 out of 5

You get a lot of computer for the low price with this laptop. I need a lightweight laptop for my business travel. Right now the hybrids and tablets cannot adequately accommodate the software that I must access and use on a regular basis. This laptop addresses my needs: 1) it is light weight, small, and portable 2) it has excellent wi-fi access [this was a major problem on my last laptop - a Sony Vaio] 3] it can accommodate my MS Office software bundle which cannot easily be done on tablets. Although there are hybrid options, they don't seem to be ready for prime time as of yet and they are pretty expensive compared to this product. 4) great price for a workhorse laptop. You won't find a better deal.

Best laptop ever I have had!

POSTED BY: Danny_Bo , Chicago, IL
Overall rating: 5 out of 5 5 out of 5

This is an affordable, light, portable, and fast lap top computer. I am a school teacher and use it for daily work.

Good Laptop for the price

POSTED BY: lcgdjg , hollsopple pa
Overall rating: 5 out of 5 5 out of 5

I was very impressed with the performance for the price. Have not had any issues with the laptop. I was so impressed with it I bought a 2nd one for my Granddaughter for school.

Love the laptop, Hate Windows 8

POSTED BY: Princess Shopper , Jacksonville, FL
Overall rating: 5 out of 5 5 out of 5

The only reason the performance rating I gave isn't 5 stars is because of Windows 8 which, frankly, I think is unstable. BUT, this is a cool laptop for the price. I like the smaller size having been used to a 17" then a 15" screen. When I upgraded to Windows 8.1, I lost the touch screen. Toshiba customer support number was accessbile from their web site, which isn't always the case with companies these days. Support was wonderful and the problem quickly resolved.

Laptop

POSTED BY: Ken
Overall rating: 5 out of 5 5 out of 5

This laptop exceeds my expectations.

Small Package, high performance

POSTED BY: Mark , Fredericksburg, VA
Overall rating: 5 out of 5 5 out of 5

I prefer a small laptop for ease of travelling with carry on luggage. My new NB15T more than meets the requirement. I also like the type AC wifi standard. Very fast throughput with my AC router.

Perfect for College

POSTED BY: Janel , Detroit, MI
Overall rating: 4 out of 5 4 out of 5

This is a perfect lightweight portable laptop for college classes.I tried a tablet but missed the efficiency and features of a laptop. This is just what I was looking for. Touchscreen is awesome. Battery life is 4 hours. Works perfectly for searching internet, streaming, downloading and uploading. Overall very satisfied! Also wanted to mention that the charger is smaller than ones I've seen which adds to lightweight portability around campus!

Issues

POSTED BY: Obtuse 1 , Roscommon, MI
Overall rating: 4 out of 5 4 out of 5

I like everything about this laptop so far, but it has some issues. I do not know what causes it, but every now and again, the screen and computer keys lock up forcing a shut down with the on/off control. the screen locks and several bubbles flash like someone is touching the screen at about 8 places on the screen and the keyboard will not function when the touch screen freezes.

Love it!

POSTED BY: jrh , Glendale, AZ
Overall rating: 4 out of 5 4 out of 5

I love the size, touch screen and the length of battery life. I can go a couple of days before recharging. Still figuring out the touch screen. Would love it if there was a stylus that worked with it.

Satellite NB15t laptop

POSTED BY: JT , St Johns, MI
Overall rating: 4 out of 5 4 out of 5

Overall it is a pretty good laptop. Windows 8.1 takes some getting used to. The touch screen ceases to function intermittently, which is why i didn't rate it 5 stars. Once past the 8.1 learning curve, and getting my software on it, it seems to be a nice little unit, very portable.

good laptop

POSTED BY: jamie , grand rapids mi,
Overall rating: 4 out of 5 4 out of 5

sometimes the touch screen acts up and when the computer updates it has a problem with connecting to my internet it will not connect automatically

Good Value

POSTED BY: Tarheelham
Overall rating: 4 out of 5 4 out of 5

The Toshiba NB15T-A1302 fits nicely the need I had for a small-display laptop for use in connrecting to digital modes on my ham radio equipment. I like the 500 gB hard drive and 4 mB of RAM, something that one doesn't normally find at this price point. The only thing I am not happy with is that it does not come with a CD/DVD drive. I have never owned a laptop that did not have one, and did not even know that they made them without CD/DVD drives. Most of what I will be using it for is on the web, and the only CD product I may have to use and I can download it to a flash drive and add it to the computer that way. The computer responds quickly and the display is very clear and crisp.

best affordable portable computer

POSTED BY: Mr. Toshiba , Chicago
Overall rating: 4 out of 5 4 out of 5

This is much better than my old 13 inches ultra thin computer. It is faster, lighter, smaller, cheaper I am a teacher and bring to my school everyday. This is the best computer I have ever had.

all I need

POSTED BY: remida , jamestown ny
Overall rating: 4 out of 5 4 out of 5

been looking for a laptop for the wife to use, this fit the program, very well satisfied, however could use a bigger battery

it's okay

POSTED BY: Staci , Rochester,NY
Overall rating: 3 out of 5 3 out of 5

updating to 8.1 is supported by this laptop. Tried and could not get it to work. I went to the trouble shooting website and it wasn't on the list of laptops that supported the upgrade.

slowed down by windows 8

POSTED BY: vorteg , jupiter, fl
Overall rating: 2 out of 5 2 out of 5

Its a nifty little notebook. I had a previous generation which was superb, but this one was so slow I had to return it--the full version of windows 8 with touch screen was too much for its processor and memory and it slowed down to a snail's pace.

Several problems

POSTED BY: Bobbie , Indiana
Overall rating: 2 out of 5 2 out of 5

I love the size, weight and it is touch screen or keyboard. I could update to 8.1 for free. I like that it has desktop screen and app screen. On the other hand we had to fix several gliches ourselves to keep everything working.

BAD EXPERIENCE

POSTED BY: funny , Greensboro, NC
Overall rating: 1 out of 5 1 out of 5

I got this computer to surf the web in my bedroom. My bedroom is about 50' from my router. When I took it to use in the bedroom the router signal would go from 4 bars to no connection. The laptop was not being moved and I had another laptop in the same location that holds 4 bars. I put less than a week for how long I have been using this product, I have owned it for almost 2Mo. but, it will not do what it was purchased for so it hasn't been used.
  • $379.99
  • See in Cart
  • Discount Shown in Shopping Cart

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

    Offer Expiration Date

    This price is a limited-time offer and will expire on the date specified.

    Please place your order before the expiration date to take advantage of this offer.

    Some prices on Toshiba Direct are below Manufacturer's Suggested Price, so we are only able to show you the final price in the shopping cart.

    Please add this product to your shopping cart to view the final savings and price.

  • $
  • $379.99
  • »

add to cart
  • Laptop summary This product is prebuilt.
  • Intel® Celeron® Processor N2810
  • Windows 8
  • 4GB DDR3L 1600MHz memory
  • Intel® Integrated Graphics
  • 500GB HDD (5400rpm, Serial ATA)
  • Sold Separately: Toshiba USB Portable DVD SuperMulti Drive
  • Intel® Dual Band Wireless-AC 3160 1x1 AC (433Mbps)
  • Bluetooth® V4.0
  • Premium US keyboard (Black)
  • Touch pad pointing device with multi touch control
  • Lithium Ion (24Wh, 3-Cell)—*Not user replaceable
  • 1-USB (3.0) port
  • 2-USB (2.0) ports
  • Accessories Added: