Satellite P305-S8904

Average Customer Rating:

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

My 2nd Toshiba Laptop

Overall rating: 5 out of 5 5 out of 5

I love it better then my 1st. My 1st laptop was a Dell and it only lasted 2 years. I will never buy any other Laptop.

Great Laptop

POSTED BY: Bob , Winston-Salem, NC
Overall rating: 5 out of 5 5 out of 5

The P305 is an excellent full function laptop. However, it is more than I need. I purchased it primaily for the large screen. I use it for accessing and sending email and doing research on the internet. I do some word processing and spread sheet development. It is definitely not light to carry but I don't have to carry it much. If I were to buy one again, I would purchase a Toshiba but a smaller model. It is a powerful machine and I am pleased with it.

Excellent Laptop Computer

POSTED BY: Tekwiz , Miami Gardens, Florida
Overall rating: 5 out of 5 5 out of 5

This PC is a well constructed, sturdy, with an elegent finish. Audio quality from the on board Harman/Kardon speakers is quite good. Battery time is also good for such a large bright screen, once the screen brightness and the power consumption options are set to minimum.

Satellite Laptop

POSTED BY: ocean-cat , Richardson, TX
Overall rating: 5 out of 5 5 out of 5

The Toshiba runs cool and can even be placed on your lap and not heat up. The screen is sharp enough to have face recognition working. The camera operates without opening up additional software, which is nicer than having to go through the media center, required by other computers I have owned. Although I don't regularly listen to radio, there is installed FM radio software with an included plug-in antenna. I would have liked bluetooth to be included; the drivers are there but not the actual hardware, so an additional bluetooth dongle will be necessary. Toshiba has an updating function, which I appreciate, but I uninstalled the Norton before it began its trial since I use other virus scanning software. The over-all speed of this computer is great and all of my programs installed even though this is the first 64 bit machine I have owned. I don't intend to do any 3-D gaming with this laptop so, for me, it's a great little laptop.

Laptop works but keyboard is a drag

Overall rating: 4 out of 5 4 out of 5

Overall this laptop is fine. The processing power for the price is fair. My biggest complaint is with the keyboard. The spacebar is VERY short so I continually hit alt keys by accident causing my cursor to go to strange places on the screen. Also, the keyboard is made of super high glossy plastic. The fingerprints are omnipresent and make the laptop look messy and "schmiery."

overall super

POSTED BY: Cheif , Milford, Ohio
Overall rating: 4 out of 5 4 out of 5

This is a replacement for a orevious satelite model,I hope the quality is even better

love laptlop

Overall rating: 4 out of 5 4 out of 5

Hate Vista, XP much better operating system

good machine

POSTED BY: rroger , douglasville,ga
Overall rating: 4 out of 5 4 out of 5

nice fetures for the price

MSRP: $849.99

not available for sale from
the toshiba online store

  • Laptop summary
  • Intel® Core™2 Duo Processor T6400
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 320GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Intel® Wi-Fi Link 5100AGN (802.11a/g/n)

shop for accessories