Satellite P305D-S8903

Average Customer Rating:

goes great with check to include

Toshiba Direct | Laptops, Notebooks, Accessories, Electronics & Projectors

Sorted by:  Rating (high to low)» Rating (low to high)» Most Recent» Most Helpful»

My New Friend

POSTED BY: Yolie , Reistertwon, MD
Overall rating: 5 out of 5 5 out of 5

I love my new laptop. My daughter and I call it the cadillac of laptops. I love the graphics. I love the speakers. I love the keyboard, and everything about it.

Toshiba Laptop Review

POSTED BY: DFlexxo , Port Orange, FL
Overall rating: 5 out of 5 5 out of 5

I bought this laptop a few weeks ago because I had a Sony Vaio laptop that was the victim of a power surge. The mother board was fried and there was nothing I could do that was affordable. I started researching new laptops, and I wanted the best thing for the price I could get. That was this Toshiba. Since I have received the laptop I have nothing but praise. It has been the best computer I have ever had. I will never not buy another Toshiba. They are the best built, most affordable, and have the best performance of any laptops out there. I definitely recommend this laptop to anyone.

Luv this laptop!

POSTED BY: Deb , Fort Worth, TX
Overall rating: 5 out of 5 5 out of 5

Awesome speed, able to multitask-yea! without impeeding speed, great resolution with webcam, keyboard is fine despite others dissing it, sound superb for skype, music and movies.

LOVE IT!!!

POSTED BY: jeff , KC, MO
Overall rating: 5 out of 5 5 out of 5

I have had this laptop for about 5 months, and it is by far the bes laptop I have had.

Great Value

POSTED BY: grouchy , Ypsilanti, Michigan
Overall rating: 4 out of 5 4 out of 5

Great value for a lap top. Only complaint is the s video output. I have an older tv and wanted to use my tv as a monitor as well. This lap top cannot use an s video output adaptor to RCA video plug. Although I ave a toshiba tv with s video input direct, that does not work either as my toshiba tv is too old for the lap top to recognize. Other than that pretty good lap top.

Perfect for Students!

POSTED BY: Raquelita
Overall rating: 4 out of 5 4 out of 5

I had been considering getting a Mac when I realized that a Toshiba would fulfill my needs just as well, and for half the price. I am a student so the price of the Toshiba fit perfectly into my budget. There are no unnecessary extras. Everything that came included in this laptop is perfect for my everyday lifestyle at school and at home.

MSRP: $849.99

not available for sale from
the toshiba online store

  • Laptop summary
  • AMD Turion™ X2 Dual-Core Mobile Processor RM-70
  • Windows Vista® Home Premium (SP1, 64-bit)
  • 4GB PC6400 DDR2 800MHz SDRAM
  • 400GB HDD (5400rpm, Serial ATA)
  • DVD-SuperMulti (+/-R double layer) with Labelflash™ drive
  • Atheros® Wireless-LAN (802.11b/g/n)

shop for accessories